#include <zb_zcl_calendar.h>
PublishCalendar command
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::calendar_name[1+12] |
The CalendarName provides a method for utilities to assign a name to the entire calendar.
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::calendar_time_reference |
This field indicates how the Start Times contained in the calendar are to be interpreted.
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::calendar_type |
An 8-bit enumeration identifying the type of calendar published in this command.
| zb_uint32_t zb_zcl_calendar_publish_calendar_payload_s::issuer_calendar_id |
Unique identifier generated by the commodity Supplier to identify a particular calendar.
| zb_uint32_t zb_zcl_calendar_publish_calendar_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::number_of_day_profiles |
Number of day profiles in the Day Profile Table.
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::number_of_seasons |
Number of entries in the Seasons Table. A value of 0x00 means no Season defined.
| zb_uint8_t zb_zcl_calendar_publish_calendar_payload_s::number_of_week_profiles |
Number of week profiles in the Week Profile Table. A value of 0x00 means no Week Profile defined.
| zb_uint32_t zb_zcl_calendar_publish_calendar_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint32_t zb_zcl_calendar_publish_calendar_payload_s::start_time |
A UTC Time field to denote the time at which the published calendar becomes valid. A start date/time of 0x00000000 shall indicate that the command should be executed immediately.