#include <zb_zcl_calendar.h>
Data Fields | |
| zb_uint32_t | provider_id |
| zb_uint32_t | issuer_calendar_id |
| zb_uint8_t | start_week_id |
| zb_uint8_t | number_of_weeks |
GetWeekProfiles command payload.
| zb_uint32_t zb_zcl_calendar_get_week_profiles_payload_s::issuer_calendar_id |
IssuerCalendarID of the calendar to which the requested Week Profiles belong.
| zb_uint8_t zb_zcl_calendar_get_week_profiles_payload_s::number_of_weeks |
An 8-bit integer which represents the maximum number of Week Profiles that the client is willing to receive in response to this command. A value of 0x00 will cause the return of all week profiles with an ID equal to or greater than the Start Week ID.
| zb_uint32_t zb_zcl_calendar_get_week_profiles_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
| zb_uint8_t zb_zcl_calendar_get_week_profiles_payload_s::start_week_id |
Unique identifier for a Week Profile generated by the commodity supplier. The Start Week ID indicates the minimum ID of Week Profiles to be returned by the corresponding PublishWeekProfile command.