#include <zb_zcl_calendar.h>
Data Fields | |
| zb_uint32_t | earliest_start_time |
| zb_uint32_t | min_issuer_event_id |
| zb_uint8_t | number_of_calendars |
| zb_uint8_t | calendar_type |
| zb_uint32_t | provider_id |
GetCalendar Command Payload
| zb_uint8_t zb_zcl_calendar_get_calendar_payload_s::calendar_type |
An 8-bit enumeration identifying the calendar type of the requested calendar.
| zb_uint32_t zb_zcl_calendar_get_calendar_payload_s::earliest_start_time |
UTC Timestamp indicating the earliest start time of calendars to be returned by the corresponding PublishCalendar command.
| zb_uint32_t zb_zcl_calendar_get_calendar_payload_s::min_issuer_event_id |
A 32-bit integer representing the minimum Issuer Event ID of calendars to be returned by the corresponding PublishCalendar command.
| zb_uint8_t zb_zcl_calendar_get_calendar_payload_s::number_of_calendars |
An 8-bit integer which represents the maximum number of PublishCalendar commands that the client is willing to receive in response to this command.
| zb_uint32_t zb_zcl_calendar_get_calendar_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.