Logo
Developing with ZBOSS for Zigbee

#include <zb_zcl_common.h>

Data Fields

zb_uint8_t src_ep
 
zb_uint8_t dst_ep
 
zb_uint16_t dst_short_addr
 
zb_uint16_t profile_id
 
zb_uint16_t cluster_id
 
zb_uint8_t cluster_role
 
zb_uint16_t attr_id
 
zb_uint16_t manuf_code
 

Detailed Description

Attribute address info structure

Field Documentation

§ attr_id

zb_uint16_t zb_zcl_attr_addr_info_s::attr_id

Attribute id

§ cluster_id

zb_uint16_t zb_zcl_attr_addr_info_s::cluster_id

Cluster id

§ cluster_role

zb_uint8_t zb_zcl_attr_addr_info_s::cluster_role

Cluster role

§ dst_ep

zb_uint8_t zb_zcl_attr_addr_info_s::dst_ep

Destination endpoint

§ dst_short_addr

zb_uint16_t zb_zcl_attr_addr_info_s::dst_short_addr

Destination short address

§ profile_id

zb_uint16_t zb_zcl_attr_addr_info_s::profile_id

Profile id

§ src_ep

zb_uint8_t zb_zcl_attr_addr_info_s::src_ep

Source endpoint


The documentation for this struct was generated from the following file: