Logo
Developing with ZBOSS for Zigbee
zb_secur_ic_get_list_resp_s Struct Reference

Response for zb_secur_ic_get_list_req. More...

#include <zboss_api.h>

Data Fields

zb_uint8_t status
 
zb_uint8_t ic_table_entries
 
zb_uint8_t start_index
 
zb_uint8_t ic_table_list_count
 

Detailed Description

Response for zb_secur_ic_get_list_req.

Field Documentation

§ ic_table_entries

zb_uint8_t zb_secur_ic_get_list_resp_s::ic_table_entries

Total number of IC table entries within the device

§ ic_table_list_count

zb_uint8_t zb_secur_ic_get_list_resp_s::ic_table_list_count

Number of received IC table entries

§ start_index

zb_uint8_t zb_secur_ic_get_list_resp_s::start_index

Starting index within the IC table

§ status

zb_uint8_t zb_secur_ic_get_list_resp_s::status

The status of the command.


The documentation for this struct was generated from the following file: