Service Discovery Bind signal parameters. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_ieee_addr_t | device_addr |
| zb_uint8_t | endpoint |
| zb_uint16_t | cluster_id |
| zb_uint8_t | commodity_type |
Service Discovery Bind signal parameters.
Contains info about the device found during Service Discovery. Stack passes this parameter to the application with signal ZB_SE_SIGNAL_SERVICE_DISCOVERY_DO_BIND
| zb_uint16_t zb_se_signal_service_discovery_bind_params_s::cluster_id |
Discovered cluster
| zb_uint8_t zb_se_signal_service_discovery_bind_params_s::commodity_type |
Commodity type (for multiple commodity networks)
| zb_ieee_addr_t zb_se_signal_service_discovery_bind_params_s::device_addr |
Long address of the device
| zb_uint8_t zb_se_signal_service_discovery_bind_params_s::endpoint |
Device endpoint