| zb_uint8_t zb_nwk_nbr_iterator_entry_s::age |
Counter value for router aging. The number of nwkLinkStatusPeriod intervals since a link status command was received.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::depth |
The network depth of this device. A value of 0x00 indicates that this device is the Zigbee coordinator for the network.
| zb_uint32_t zb_nwk_nbr_iterator_entry_s::device_timeout |
Configured end device timeout, in seconds.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::device_type |
Neighbor device type -
| zb_ieee_addr_t zb_nwk_nbr_iterator_entry_s::ieee_addr |
Long address (EUI64) of the device.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::keepalive_received |
This value indicates at least one keepalive has been received from the end device since the router has rebooted.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::lqi |
Link quality. Also used to calculate incoming cost
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::mac_iface_idx |
An index into the MAC Interface Table indicating what interface the neighbour or child is bound to.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::outgoing_cost |
The cost of an outgoing link. Got from link status.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::relationship |
The relationship between the neighbour and the current device. This field shall be present in every neighbour table entry.
| zb_int8_t zb_nwk_nbr_iterator_entry_s::rssi |
Received signal strength indicator
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::rx_on_when_idle |
Indicates if neighbour receiver enabled during idle periods: TRUE = Receiver is on FALSE = Receiver is off This field should be present for entries that record the parent or children of a Zigbee router or Zigbee coordinator.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::send_via_routing |
That field is deprecated. Removed from zb_neighbor_tbl_ent_t, always 0 here.
| zb_uint16_t zb_nwk_nbr_iterator_entry_s::short_addr |
Short address (network address) of the device.
| zb_uint32_t zb_nwk_nbr_iterator_entry_s::timeout_counter |
Timeout value ED aging, in milliseconds.
| zb_uint8_t zb_nwk_nbr_iterator_entry_s::transmit_failure_cnt |
Transmit failure counter (used to initiate device address search).