Logo
Developing with ZBOSS for Zigbee
zb_leg_buf_s Struct Reference

#include <zboss_api_buf.h>

Data Fields

union {
   zb_buf_hdr_t   hdr
 
   struct zb_buf_s *   next
 
u
 
zb_uint8_t buf [ZB_IO_BUF_SIZE]
 

Detailed Description

Packet buffer (legacy)

Field Documentation

§ buf

zb_uint8_t zb_leg_buf_s::buf[ZB_IO_BUF_SIZE]

Data

§ hdr

zb_buf_hdr_t zb_leg_buf_s::hdr

Buffer header, if buffer is used

§ next

struct zb_buf_s* zb_leg_buf_s::next

Ref to next free buffer, if buffer is not used

§ u

union { ... } zb_leg_buf_s::u

Buffer header


The documentation for this struct was generated from the following file: