Logo
Developing with ZBOSS for Zigbee
zb_buf_hdr_s Struct Reference

#include <zboss_api_buf.h>

Data Fields

zb_ret_t status
 
zb_uint16_t len
 
zb_uint16_t data_offset
 
zb_uint8_t multiplicity
 
zb_uint8_t handle
 
zb_bitfield_t is_in_buf:1
 
zb_bitfield_t encrypt_type:3
 
zb_bitfield_t use_same_key:1
 
zb_bitfield_t zdo_cmd_no_resp:1
 
zb_bitfield_t is_rx_buf:1
 
zb_bitfield_t has_aps_payload:1
 
zb_bitfield_t has_aps_user_payload:1
 
zb_bitfield_t tail_len:7
 

Detailed Description

Packet buffer header.

Field Documentation

§ data_offset

zb_uint16_t zb_buf_hdr_s::data_offset

data offset in buffer buf

§ encrypt_type

zb_bitfield_t zb_buf_hdr_s::encrypt_type

payload must be encrypted before send, if !0.

See also
zb_secur_buf_encr_type_e.

§ handle

zb_uint8_t zb_buf_hdr_s::handle

The handle associated with the NSDU to be transmitted by the NWK layer entity.

§ has_aps_payload

zb_bitfield_t zb_buf_hdr_s::has_aps_payload

if 1, than packet comes from APS, the flag is needed to increase APS packets counter in diagnostic data on packet sending

§ has_aps_user_payload

zb_bitfield_t zb_buf_hdr_s::has_aps_user_payload

if 1, than packet comes with APS user's payload

§ is_in_buf

zb_bitfield_t zb_buf_hdr_s::is_in_buf

if 1, this is input buffer

§ is_rx_buf

zb_bitfield_t zb_buf_hdr_s::is_rx_buf

if 1, this is buffer with received packet and nwk_mac_addrs_t is at buffer tail

§ len

zb_uint16_t zb_buf_hdr_s::len

current layer buffer length

§ multiplicity

zb_uint8_t zb_buf_hdr_s::multiplicity

if greater that 1, then the following (multiplicity - 1) buffers are occupied with payload data and should not be treated as having valid headers, etc.

§ status

zb_ret_t zb_buf_hdr_s::status

some status to be passed with packet

§ tail_len

zb_bitfield_t zb_buf_hdr_s::tail_len

the length of the perameters section

§ use_same_key

zb_bitfield_t zb_buf_hdr_s::use_same_key

if 1, use same nwk key packet was encrypted by

§ zdo_cmd_no_resp

zb_bitfield_t zb_buf_hdr_s::zdo_cmd_no_resp

if 1, this is ZDO command with no response - call callback at confirm


The documentation for this struct was generated from the following file: