Logo
Developing with ZBOSS for Zigbee
zb_apsme_remove_all_groups_conf_s Struct Reference

APSME-REMOVE-ALL-GROUPS.confirm primitive parameters. More...

#include <zboss_api_aps.h>

Data Fields

zb_uint8_t endpoint
 
zb_ret_t status
 

Detailed Description

APSME-REMOVE-ALL-GROUPS.confirm primitive parameters.

Field Documentation

§ endpoint

zb_uint8_t zb_apsme_remove_all_groups_conf_s::endpoint

The endpoint which is to be removed from all groups.

§ status

zb_ret_t zb_apsme_remove_all_groups_conf_s::status

The status of the request to remove all groups.


The documentation for this struct was generated from the following file: