Logo
Developing with ZBOSS for Zigbee

APSME-ADD-GROUP.request primitive parameters, should be passed to zb_zdo_add_group_req() More...

#include <zboss_api_aps.h>

Data Fields

zb_uint16_t group_address
 
zb_uint8_t endpoint
 
zb_callback_t confirm_cb
 

Detailed Description

APSME-ADD-GROUP.request primitive parameters, should be passed to zb_zdo_add_group_req()

Field Documentation

§ confirm_cb

zb_callback_t zb_apsme_add_group_req_s::confirm_cb

The callback to be called when the operation is completed.

§ endpoint

zb_uint8_t zb_apsme_add_group_req_s::endpoint

The endpoint to which the given group is being added.

§ group_address

zb_uint16_t zb_apsme_add_group_req_s::group_address

The 16-bit address of the group being added.


The documentation for this struct was generated from the following file: