Logo
Developing with ZBOSS for Zigbee
zb_af_node_power_desc_s Struct Reference

#include <zboss_api_af.h>

Data Fields

zb_uint16_t power_desc_flags
 

Detailed Description

Node power descriptor

Field Documentation

§ power_desc_flags

zb_uint16_t zb_af_node_power_desc_s::power_desc_flags

Field name Bits Current power mode: 4
Available power sources: 4
Current power source: 4
Current power source level: 4


The documentation for this struct was generated from the following file: