Logo
Developing with ZBOSS for Zigbee

#include <zboss_api_af.h>

Data Fields

zb_uint16_t node_desc_flags
 
zb_uint8_t mac_capability_flags
 
zb_uint16_t manufacturer_code
 
zb_uint8_t max_buf_size
 
zb_uint16_t max_incoming_transfer_size
 
zb_uint16_t server_mask
 
zb_uint16_t max_outgoing_transfer_size
 
zb_uint8_t desc_capability_field
 

Detailed Description

Node descriptor

Field Documentation

§ desc_capability_field

zb_uint8_t zb_af_node_desc_s::desc_capability_field

Descriptor capability field

§ mac_capability_flags

zb_uint8_t zb_af_node_desc_s::mac_capability_flags

mac capability

§ manufacturer_code

zb_uint16_t zb_af_node_desc_s::manufacturer_code

Manufacturer code

§ max_buf_size

zb_uint8_t zb_af_node_desc_s::max_buf_size

Maximum buffer size

§ max_incoming_transfer_size

zb_uint16_t zb_af_node_desc_s::max_incoming_transfer_size

Maximum incoming transfer size

§ max_outgoing_transfer_size

zb_uint16_t zb_af_node_desc_s::max_outgoing_transfer_size

Maximum outgoing transfer size

§ node_desc_flags

zb_uint16_t zb_af_node_desc_s::node_desc_flags

node description

§ server_mask

zb_uint16_t zb_af_node_desc_s::server_mask

Server mask


The documentation for this struct was generated from the following file: