Data Structures | |
| struct | zgp_to_zb_cmd_mapping_s |
| Mapping of ZGPD command ID to Zigbee ZCL command ID. More... | |
| struct | zb_zgps_mapping_entry_additional_info_option_selector_s |
| Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_generic_switch_option_data_s |
| Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_generic_switch_option_s |
| Mapping table entry additional info generic switch option structure. More... | |
| struct | zb_zgps_mapping_entry_additional_info_option_record_s |
| Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_additional_info_s |
| Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_s |
| Mapping table entry structure. More... | |
Macros | |
| #define | ZB_ZGP_ZCL_CMD_ID_UNDEFINED (0xff) |
| #define | ZB_ZGP_ZCL_CLUSTER_ID_UNDEFINED (0xffff) |
| #define | ZB_GPDF_CMD_UNDEFINED (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_PASS_RAW_GPDF_TO_APP (0xfc) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_NO_PAIRS (0xfd) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_ALL_ARE_MATCHED (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_NO_PAYLOAD (0x00) |
| #define | ZB_ZGP_MAPPING_ENTRY_GPDF_PAYLOAD (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_PARSED_PAYLOAD (0xfe) |
| #define | ZB_ZGP_MAPPING_ENTRY_OPTIONS(app_id, add_info_present) (((((add_info_present) & 0x01) << 3)) | ((app_id) & 0x07)) |
| #define | ZB_ZGP_MAPPING_ENTRY_OPTIONS_IS_ADDITIONAL_INFO_PRESENT(options) (((options) >> 3) & 0x01) |
| #define | ZB_ZGP_GET_MAPPING_ENTRY_ZCL_PAYLOAD_PTR(entry) (&entry->zcl_payload_length+sizeof(entry->zcl_payload_length)) |
| #define | ZB_ZGP_SET_MAPPING_TABLE(table_ptr, table_size_ptr) |
| Set mapping table information that is used to fill ZGP command - ZCL cluster mapping table. More... | |
| #define | ZB_ZGP_REGISTER_COMM_REQ_CB(cb) |
| Register commissioning request callback. More... | |
| #define | ZB_ZGP_REGISTER_APP_CIC_CB(cb) |
| Register application commissioning indication callback. More... | |
| #define | ZB_ZGP_FILL_GPS_SECURITY_LEVEL(sec_lvl, with_link_key, involve_tc) (((sec_lvl) & 3U) | ((!!(with_link_key)) << 2U) | ((!!(involve_tc)) << 3U)) |
Typedefs | |
| typedef struct zgp_to_zb_cmd_mapping_s | zgp_to_zb_cmd_mapping_t |
| Mapping of ZGPD command ID to Zigbee ZCL command ID. | |
| typedef struct zb_zgps_mapping_entry_additional_info_option_selector_s | zb_zgps_mapping_entry_additional_info_option_selector_t |
| Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry. | |
| typedef struct zb_zgps_mapping_entry_generic_switch_option_data_s | zb_zgps_mapping_entry_generic_switch_option_data_t |
| Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. | |
| typedef struct zb_zgps_mapping_entry_generic_switch_option_s | zb_zgps_mapping_entry_generic_switch_option_t |
| Mapping table entry additional info generic switch option structure. | |
| typedef struct zb_zgps_mapping_entry_additional_info_option_record_s | zb_zgps_mapping_entry_additional_info_option_record_t |
| Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry. | |
| typedef struct zb_zgps_mapping_entry_additional_info_s | zb_zgps_mapping_entry_additional_info_t |
| Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry. | |
| typedef struct zb_zgps_mapping_entry_s | zb_zgps_mapping_entry_t |
| Mapping table entry structure. | |
| typedef void(* | zb_zgp_app_comm_ind_cb_t) (zb_zgpd_id_t *zgpd_id, zb_uint8_t param) |
| Application callback, indication of the attempted commissioning in GPS operational mode. More... | |
Enumerations | |
| enum | zb_zgps_mapping_entry_8bit_vector_option_ids_e { ZB_ZGPS_MAPPING_ENTRY_8BIT_VECTOR_OPTION_ID_GENERIC_SWITCH_COMMAND_EXECUTION = 0U } |
| A.3.6.2.2.1.1 OptionIDs for GPD 8-bit vector commands. | |
| enum | zb_zgps_mapping_entry_compact_attr_report_option_ids_e { ZB_ZGPS_MAPPING_ENTRY_COMPACT_ATTR_REPORT_REPORTABLE = 0U } |
| A.3.6.2.2.1.2 OptionIDs for GPD Compact Attribute Reporting. | |
Functions | |
| void | zb_zgps_start_commissioning (zb_time_t timeout) |
| Put ZGPS into commissioning mode, the mode will be changed back to operational mode if: More... | |
| void | zb_zgps_start_commissioning_on_ep (zb_uint8_t ep, zb_time_t timeout) |
| Put ZGPS into commissioning mode on a specific endpoint. More... | |
| void | zb_zgps_stop_commissioning (void) |
| Switch ZGPS back to operational mode from commissioning. More... | |
| void | zb_zgps_accept_commissioning (zb_bool_t accept) |
| Accept/reject ZGPD commissioning attempt. More... | |
| void | zb_zgps_delete_zgpd (zb_uint8_t buf_ref, zb_zgpd_id_t *zgpd_id) |
| Remove all the information about ZGPD from stack. More... | |
| void | zb_zgps_delete_all_zgpd (void) |
| Remove all the information about ALL ZGPD from stack. | |
| void | zb_zgps_get_diag_data (zb_zgpd_id_t *zgpd_id, zb_uint8_t *lqi, zb_int8_t *rssi) |
| void | zb_zgps_set_security_level (zb_uint_t level) |
| zb_uint8_t | zb_zgps_get_security_level (void) |
| void | zb_zgp_set_shared_security_key_type (zb_uint_t key_type) |
| void | zb_zgp_set_shared_security_key (zb_uint8_t *key) |
| void | zb_zgps_set_commissioning_exit_mode (zb_uint_t cem) |
| void | zb_zgps_set_communication_mode (zgp_communication_mode_t mode) |
| zb_ret_t | zb_zgp_convert_8bit_vector (zb_uint8_t vector_8bit_cmd_id, zb_uint8_t switch_type, zb_uint8_t num_of_contacts, zb_uint8_t contact_status, zb_uint8_t *zgp_cmd_out) |
| void | zb_zgp_gpdf_raw_indication (zb_bufid_t buf_ref) |
| Application function to override allows custom handling incoming raw GPDF packet. More... | |
| void | zb_zgp_set_skip_gpdf (zb_uint8_t skip) |
| zb_uint8_t | zb_zgp_get_skip_gpdf (void) |
| void | zb_zgp_sync_pib (zb_uint8_t param) |
| #define ZB_ZGP_FILL_GPS_SECURITY_LEVEL | ( | sec_lvl, | |
| with_link_key, | |||
| involve_tc | |||
| ) | (((sec_lvl) & 3U) | ((!!(with_link_key)) << 2U) | ((!!(involve_tc)) << 3U)) |
Fill security level constant to be passed to zb_zgps_set_security_level()
Described in A.3.3.2.6 gpsSecurityLevel attribute.
| sec_lvl | zb_zgp_security_level_e Minimal GPD Security Level sub-field contains the minimum gpdSecurityLevel this sink accepts |
| with_link_key | 1 bit - Protection with the gpLinkKey sub-field, indicates if the GPDs attempting the pairing are required to support protecting the over-the-air exchange of the GPD Key |
| involve_tc | always zero for the current GPPB specification |
| #define ZB_ZGP_REGISTER_APP_CIC_CB | ( | cb | ) |
Register application commissioning indication callback.
| cb | [in] Application commissioning indication callback (zb_zgp_app_comm_ind_cb_t) |
| #define ZB_ZGP_REGISTER_COMM_REQ_CB | ( | cb | ) |
Register commissioning request callback.
| cb | [in] Commissioning request callback (zb_zgp_comm_req_cb_t) |
| #define ZB_ZGP_SET_MAPPING_TABLE | ( | table_ptr, | |
| table_size_ptr | |||
| ) |
Set mapping table information that is used to fill ZGP command - ZCL cluster mapping table.
| [in] | table_ptr | Mapping information, pointer to array of type zb_zgps_mapping_entry_t |
| [in] | table_size_ptr | pointer to size of the table - max entry number what can be iterated |
| typedef void( * zb_zgp_app_comm_ind_cb_t) (zb_zgpd_id_t *zgpd_id, zb_uint8_t param) |
Application callback, indication of the attempted commissioning in GPS operational mode.
Application commissioning indication callback notifies application about commissioning attempt from ZGPD. Callback is called when commissioning frame or notification is received from ZGPD. Callback provides to zgpd_id and full incoming packet's data. Based on these parameters user application should decide further actions.
Application commissioning indication callback should be set during ZGP initialization using ZB_ZGP_REGISTER_APP_CIC_CB macro.
| zgpd_id | [in] ZGPD ID |
| param | [in] buffer index, containing GPDF |
| zb_ret_t zb_zgp_convert_8bit_vector | ( | zb_uint8_t | vector_8bit_cmd_id, |
| zb_uint8_t | switch_type, | ||
| zb_uint8_t | num_of_contacts, | ||
| zb_uint8_t | contact_status, | ||
| zb_uint8_t * | zgp_cmd_out | ||
| ) |
Application function to override translation of 8-bit vector command (generic switch)
If this function is not implemented in the application, then ZBOSS performs a default translation as recommended by ZGP spec (see Green Power Basic specification v1.1.1, tables 51, 52). If there is no default translation found, then the received command is dropped.
If this function is implemented by the the application, then application is fully responsible for a translation of GPD 8-bit vector commands. For any return code but RET_OK, ZBOSS will stop command processing and drop it.
Note: The translation is done to GPDF command ID, not to ZCL command ID.
| [in] | vector_8bit_cmd_id | incoming command ID: press (0x69) or release(0x6a) |
| [in] | switch_type | switch type of the command's originator (see ZGP spec. A.4.2.1.1.10) |
| [in] | num_of_contacts | number of contacts command's originator provides |
| [in] | contact_status | contacts status from the payload of the received command |
| [out] | zgp_cmd_out | GPDF command ID to which incoming command should be translated |
See Green Power Basic specification v1.1.1, chapters A.3.6.2.2.2, A.4.2.2.1 for more information.
| void zb_zgp_gpdf_raw_indication | ( | zb_bufid_t | buf_ref | ) |
Application function to override allows custom handling incoming raw GPDF packet.
If this function os not implemented by the application, then ZBOSS drops the buffer without any additional handling.
If this function is implemented by the application, the application itself shall carry to free this resource.
| buf_ref |
| void zb_zgp_set_shared_security_key | ( | zb_uint8_t * | key | ) |
Set gpSharedSecurityKey GP cluster attribute
Described in A.3.3.3.1 gpSharedSecurityKey attribute.
| key | Security key to set |
| void zb_zgp_set_shared_security_key_type | ( | zb_uint_t | key_type | ) |
Set gpSharedSecurityKeyType GP cluster attribute
Described in A.3.3.3.1 gpSharedSecurityKeyType attribute.
| key_type | Security key type to set ( |
| void zb_zgp_set_skip_gpdf | ( | zb_uint8_t | skip | ) |
Set ZBOSS to skip all incoming GPDF.
To be used for testing only. Use that function with ZB_TRUE parameter to prevent Combo device from receiving GPDFS thus always working thru Proxy device.
| skip | if ZB_TRUE, skip incoming GP frames |
| void zb_zgps_accept_commissioning | ( | zb_bool_t | accept | ) |
Accept/reject ZGPD commissioning attempt.
This function should be called as an answer to commissioning request made by stack via signal ZB_ZGP_SIGNAL_APPROVE_COMMISSIONING or zb_zgp_comm_req_cb_t callback. Also, it can be called from zb_zgp_comm_req_cb_t callback as well as outside it.
| [in] | accept | - If ZB_TRUE, then stack will continue ongoing commissioning process with ZGPD Otherwise ongoing commissioning process will be terminated |
| void zb_zgps_delete_zgpd | ( | zb_uint8_t | buf_ref, |
| zb_zgpd_id_t * | zgpd_id | ||
| ) |
Remove all the information about ZGPD from stack.
In ZGP there is no way to say ZGPD to leave the network. ZGPD can leave network by itself using "Decommissioning" command, but ZGPS can miss this command if it was not in commissioning state.
This function removes all the information related to specified ZGPD from stack.
| buf_ref | reference to the free buffer |
| zgpd_id | identifier of ZGPD to be removed |
| void zb_zgps_get_diag_data | ( | zb_zgpd_id_t * | zgpd_id, |
| zb_uint8_t * | lqi, | ||
| zb_int8_t * | rssi | ||
| ) |
Get LQI and RSSI last time received from that ZGPD.
| zb_uint8_t zb_zgps_get_security_level | ( | void | ) |
Get gpsSecurityLevel GP cluster attribute of gpcb
Described in A.3.3.2.6 gpsSecurityLevel attribute.
| void zb_zgps_set_commissioning_exit_mode | ( | zb_uint_t | cem | ) |
Set gpsCommissioningExitMode GP cluster attribute
Described in A.3.3.2.4 gpsCommissioningExitMode attribute.
| cem | Commissioning exit mode to set ( |
| void zb_zgps_set_communication_mode | ( | zgp_communication_mode_t | mode | ) |
Set gpsCommunicationMode GP cluster attribute of gpcb
Described in A.3.3.2.3 gpsCommunicationMode attribute
| mode | zgp_communication_mode_t communication mode |
| void zb_zgps_set_security_level | ( | zb_uint_t | level | ) |
Set gpsSecurityLevel GP cluster attribute of gpcb
Described in A.3.3.2.6 gpsSecurityLevel attribute.
| level | Security level to set |
| void zb_zgps_start_commissioning | ( | zb_time_t | timeout | ) |
Put ZGPS into commissioning mode, the mode will be changed back to operational mode if:
ZB_ZGP_SIGNAL_MODE_CHANGE is generated when sink changes mode from Operation Mode to Commissioning Mode and when it changes from Commissioning Mode to Operational Mode.
ZB_ZGP_SIGNAL_COMMISSIONING is generated if a successful commission happens or if a decommissioning happens
| timeout | Maximum commissioning time in beacon intervals, 0 means no timeout. |
It is safe to call this function when device is already in commissioning mode. In this case function does nothing.
| void zb_zgps_start_commissioning_on_ep | ( | zb_uint8_t | ep, |
| zb_time_t | timeout | ||
| ) |
Put ZGPS into commissioning mode on a specific endpoint.
It is safe to call this function when device is already in commissioning mode. In this case function does nothing.
| [in] | ep | Endpoint to start a commissioning. Will be used for GPD command forwarding |
| [in] | timeout | Maximum commissioning time in beacon intervals. 0 means no timeout. If timeout occurs, then result of commissioning is ZB_ZGP_COMMISSIONING_TIMED_OUT |
| void zb_zgps_stop_commissioning | ( | void | ) |
Switch ZGPS back to operational mode from commissioning.