Logo
Developing with ZBOSS for Zigbee
Write attributes command sending and parsing.

Data Structures

struct  zb_zcl_write_attr_req_s
 ZCL Write Attribute Command frame. More...
 
struct  zb_zcl_write_attr_res_s
 ZCL Write Attribute Command frame. More...
 

Macros

#define ZB_ZCL_GENERAL_GET_NEXT_WRITE_ATTR_REQ(data_ptr, data_len, write_attr_req)
 Parses Write attribute request and returns next Write attribute record or NULL if there is no more data. More...
 
#define ZB_ZCL_GET_NEXT_WRITE_ATTR_RES(data_buf, write_attr_resp)
 Parses Write attribute response and returns next Write attribute status or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE(buffer, cmd_ptr, def_resp, write_attr_type)
 Initialize Write attribute command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ(buffer, cmd_ptr, def_resp)
 Initialize Write attribute command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_MANUF(buffer, cmd_ptr, direction, def_resp, manuf_code)
 Initialize Write attribute command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_NO_RESP(buffer, cmd_ptr, def_resp)
 Initialize Write Attribute No Response command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_UNDIV(buffer, cmd_ptr, def_resp)
 Initialize Write Attribute Undivided command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_A(buffer, cmd_ptr, direction, def_resp)
 Initialize Write attribute command. More...
 
#define ZB_ZCL_GENERAL_ADD_VALUE_WRITE_ATTR_REQ(cmd_ptr, attr_id, attr_type, attr_val)
 Add attribute value to command payload. More...
 
#define ZB_ZCL_GENERAL_SEND_WRITE_ATTR_REQ( buffer, cmd_ptr, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb)
 Send Write attribute command. More...
 
#define ZB_ZCL_GENERAL_SEND_WRITE_ATTRS_REQ( buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id)
 Send "write attributes" request. deprecate. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP(_buffer, _cmd_ptr, _seq)
 Initialize Write attribute response command. More...
 
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP_EXT(_buffer, _cmd_ptr, _direction, _seq, _is_manuf, _manuf_id)
 Initialize Write attribute response command. More...
 
#define ZB_ZCL_GENERAL_SUCCESS_WRITE_ATTR_RESP(_cmd_ptr)
 Add Success status value to Write attribute response command payload. More...
 
#define ZB_ZCL_GENERAL_SEND_WRITE_ATTR_RESP( _buffer, _cmd_ptr, _addr, _dst_addr_mode, _dst_ep, _ep, _profile_id, _cluster_id, _cb)
 Send Write attribute response command. More...
 

Typedefs

typedef struct zb_zcl_write_attr_req_s zb_zcl_write_attr_req_t
 ZCL Write Attribute Command frame. More...
 
typedef struct zb_zcl_write_attr_res_s zb_zcl_write_attr_res_t
 ZCL Write Attribute Command frame. More...
 

Detailed Description

Both write attributes request and response commands have variable-length payload.

Write attributes request can be filled as following:

On the server side, this packet could be parsed in the following manner:

zb_zcl_write_attr_req_t *write_attr_req;
...
do
{
ZB_ZCL_GENERAL_GET_NEXT_WRITE_ATTR_REQ(data_buf, write_attr_req);
if (write_attr_req)
{
process write attribute request record
}
}
while(write_attr_req);

Response sending and parsing could be done in the same manner.

Macro Definition Documentation

§ ZB_ZCL_GENERAL_ADD_VALUE_WRITE_ATTR_REQ

#define ZB_ZCL_GENERAL_ADD_VALUE_WRITE_ATTR_REQ (   cmd_ptr,
  attr_id,
  attr_type,
  attr_val 
)
Value:
{ \
ZB_ZCL_PACKET_PUT_DATA16_VAL(cmd_ptr, (attr_id)); \
ZB_ZCL_PACKET_PUT_DATA8(cmd_ptr, (attr_type)); \
(cmd_ptr) = zb_zcl_put_value_to_packet(cmd_ptr, attr_type, attr_val); \
}
zb_uint8_t * zb_zcl_put_value_to_packet(zb_uint8_t *cmd_ptr, zb_uint8_t attr_type, zb_uint8_t *attr_value)

Add attribute value to command payload.

Parameters
cmd_ptr- pointer to a command data memory
attr_id- attribute identifier
attr_type- attribute type
attr_val- pointer to attribute data value

§ ZB_ZCL_GENERAL_GET_NEXT_WRITE_ATTR_REQ

#define ZB_ZCL_GENERAL_GET_NEXT_WRITE_ATTR_REQ (   data_ptr,
  data_len,
  write_attr_req 
)

Parses Write attribute request and returns next Write attribute record or NULL if there is no more data.

If request contains invalid data, NULL is returned.

Parameters
data_ptr- pointer to the data of a zb_bufid_t buffer containing write attribute request data
data_len- variable containing length of a zb_bufid_t buffer
write_attr_req- out pointer to zb_zcl_write_attr_req_t, containing Write attribute record
Note
buffer data by data_ptr should contain Write attribute request payload, without ZCL header.

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ (   buffer,
  cmd_ptr,
  def_resp 
)
Value:
(buffer), (cmd_ptr), (def_resp), ZB_ZCL_CMD_WRITE_ATTRIB);
#define ZB_ZCL_CMD_WRITE_ATTRIB
Definition: zb_zcl_commands.h:68
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE(buffer, cmd_ptr, def_resp, write_attr_type)
Initialize Write attribute command.
Definition: zb_zcl_commands.h:981

Initialize Write attribute command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_A

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_A (   buffer,
  cmd_ptr,
  direction,
  def_resp 
)
Value:
{ \
cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A(cmd_ptr, direction, ZB_ZCL_NOT_MANUFACTURER_SPECIFIC, def_resp); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_WRITE_ATTRIB); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_CMD_WRITE_ATTRIB
Definition: zb_zcl_commands.h:68
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1013

Initialize Write attribute command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
direction- direction of command (see zcl_frame_direction)
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE (   buffer,
  cmd_ptr,
  def_resp,
  write_attr_type 
)
Value:
{ \
cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL(cmd_ptr, def_resp); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), write_attr_type); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543

Initialize Write attribute command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
def_resp- enable/disable default response
write_attr_type- type of 'Write Attribute' command: default -
See also
ZB_ZCL_CMD_WRITE_ATTRIB; no response -
ZB_ZCL_CMD_WRITE_ATTRIB_NO_RESP; undivided -
ZB_ZCL_CMD_WRITE_ATTRIB_UNDIV;

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_MANUF

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_MANUF (   buffer,
  cmd_ptr,
  direction,
  def_resp,
  manuf_code 
)
Value:
{ \
cmd_ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
cmd_ptr, direction, ZB_ZCL_MANUFACTURER_SPECIFIC, def_resp); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_EXT( \
cmd_ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_TRUE, manuf_code, ZB_ZCL_CMD_WRITE_ATTRIB); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_CMD_WRITE_ATTRIB
Definition: zb_zcl_commands.h:68
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1016
#define ZB_TRUE
Definition: zb_types.h:350

Initialize Write attribute command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
direction- direction of command (see zcl_frame_direction)
def_resp- enable/disable default response
manuf_code- manufacturer specific code

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_NO_RESP

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_NO_RESP (   buffer,
  cmd_ptr,
  def_resp 
)
Value:
(buffer), (cmd_ptr), (def_resp), ZB_ZCL_CMD_WRITE_ATTRIB_NO_RESP);
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE(buffer, cmd_ptr, def_resp, write_attr_type)
Initialize Write attribute command.
Definition: zb_zcl_commands.h:981
#define ZB_ZCL_CMD_WRITE_ATTRIB_NO_RESP
Definition: zb_zcl_commands.h:71

Initialize Write Attribute No Response command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_UNDIV

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_UNDIV (   buffer,
  cmd_ptr,
  def_resp 
)
Value:
(buffer), (cmd_ptr), (def_resp), ZB_ZCL_CMD_WRITE_ATTRIB_UNDIV);
#define ZB_ZCL_CMD_WRITE_ATTRIB_UNDIV
Definition: zb_zcl_commands.h:69
#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_REQ_BY_TYPE(buffer, cmd_ptr, def_resp, write_attr_type)
Initialize Write attribute command.
Definition: zb_zcl_commands.h:981

Initialize Write Attribute Undivided command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP (   _buffer,
  _cmd_ptr,
  _seq 
)
Value:
{ \
cmd_ptr = ZB_ZCL_START_PACKET((_buffer)); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_RESP_FRAME_CONTROL((_cmd_ptr)); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER((_cmd_ptr), (_seq), ZB_ZCL_CMD_WRITE_ATTRIB_RESP); \
}
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_CMD_WRITE_ATTRIB_RESP
Definition: zb_zcl_commands.h:70

Initialize Write attribute response command.

Parameters
_buffer- buffer to store command data
_cmd_ptr- pointer to a command data memory
_seq- command sequence

§ ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP_EXT

#define ZB_ZCL_GENERAL_INIT_WRITE_ATTR_RESP_EXT (   _buffer,
  _cmd_ptr,
  _direction,
  _seq,
  _is_manuf,
  _manuf_id 
)
Value:
{ \
cmd_ptr = ZB_ZCL_START_PACKET((_buffer)); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_RESP_FRAME_CONTROL_A((_cmd_ptr), (_direction), (_is_manuf)); \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_EXT((_cmd_ptr), (_seq), (_is_manuf), (_manuf_id), ZB_ZCL_CMD_WRITE_ATTRIB_RESP); \
}
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_CMD_WRITE_ATTRIB_RESP
Definition: zb_zcl_commands.h:70

Initialize Write attribute response command.

Parameters
_buffer- buffer to store command data
_cmd_ptr- pointer to a command data memory
_direction- direction of command (see zcl_frame_direction)
_seq- command sequence
_is_manuf- whether command is manufacturer specific
_manuf_id- manufacturer ID (needed if _is_manuf is set)

§ ZB_ZCL_GENERAL_SEND_WRITE_ATTR_REQ

#define ZB_ZCL_GENERAL_SEND_WRITE_ATTR_REQ (   buffer,
  cmd_ptr,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  profile_id,
  cluster_id,
  cb 
)
Value:
{ \
ZB_ZCL_FINISH_PACKET(buffer, cmd_ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, profile_id, cluster_id, cb); \
}

Send Write attribute command.

Parameters
buffer- buffer to store command data
cmd_ptr- pointer to a command data memory
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
profile_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

§ ZB_ZCL_GENERAL_SEND_WRITE_ATTR_RESP

#define ZB_ZCL_GENERAL_SEND_WRITE_ATTR_RESP (   _buffer,
  _cmd_ptr,
  _addr,
  _dst_addr_mode,
  _dst_ep,
  _ep,
  _profile_id,
  _cluster_id,
  _cb 
)
Value:
{ \
ZB_ZCL_FINISH_PACKET((_buffer), (_cmd_ptr)) \
ZB_ZCL_SEND_COMMAND_SHORT((_buffer), (_addr), (_dst_addr_mode), (_dst_ep), (_ep), \
(_profile_id), (_cluster_id), (_cb)); \
}

Send Write attribute response command.

Parameters
_buffer- buffer to store command data
_cmd_ptr- pointer to a command data memory
_addr- address to send packet to
_dst_addr_mode- addressing mode
_dst_ep- destination endpoint
_ep- sending endpoint
_profile_id- profile identifier
_cluster_id- cluster identifier
_cb- callback for getting command send status

§ ZB_ZCL_GENERAL_SEND_WRITE_ATTRS_REQ

#define ZB_ZCL_GENERAL_SEND_WRITE_ATTRS_REQ (   buffer,
  addr,
  addr_mode,
  dst_ep,
  ep,
  prof_id,
  cluster_id 
)
Value:
ZB_ZCL_SEND_GENERAL_COMMAND_REQ_SHORT( \
buffer, addr, addr_mode, dst_ep, ep, prof_id, cluster_id, ZB_ZCL_CMD_WRITE_ATTRIB)
#define ZB_ZCL_CMD_WRITE_ATTRIB
Definition: zb_zcl_commands.h:68

Send "write attributes" request. deprecate.

§ ZB_ZCL_GENERAL_SUCCESS_WRITE_ATTR_RESP

#define ZB_ZCL_GENERAL_SUCCESS_WRITE_ATTR_RESP (   _cmd_ptr)
Value:
{ \
ZB_ZCL_PACKET_PUT_DATA8((_cmd_ptr), ZB_ZCL_STATUS_SUCCESS); \
}
#define ZB_ZCL_STATUS_SUCCESS
Definition: zb_zcl_common.h:360

Add Success status value to Write attribute response command payload.

Parameters
_cmd_ptr- pointer to a command data memory

§ ZB_ZCL_GET_NEXT_WRITE_ATTR_RES

#define ZB_ZCL_GET_NEXT_WRITE_ATTR_RES (   data_buf,
  write_attr_resp 
)

Parses Write attribute response and returns next Write attribute status or NULL if there is no more data.

If response contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing write attribute response data
write_attr_resp- out pointer to zb_zcl_write_attr_res_t, containing Write attribute status
Note
data_buf buffer should contain Write attribute response payload, without ZCL header. Each parsed Write attribute response is extracted from initial data_buf buffer

Typedef Documentation

§ zb_zcl_write_attr_req_t

ZCL Write Attribute Command frame.

See also
ZCL spec, 2.4.3 Write Attributes Command

§ zb_zcl_write_attr_res_t

ZCL Write Attribute Command frame.

See also
ZCL spec, 2.4.3 Write Attributes Command