Functions | |
| void | zb_secur_setup_nwk_key (zb_uint8_t *key, zb_uint8_t i) |
| Setup NWK key from the application level manually. More... | |
| void | zb_secur_nwk_key_switch_procedure (zb_uint8_t param) |
| void zb_secur_nwk_key_switch_procedure | ( | zb_uint8_t | param | ) |
Initiate procedure of NWK key switching.
Generate next NWK key if it not exists, broadcast new NWK key, after delay broadcast NWK key switch command. Can run at TC only.
| param | - work buffer ID or 0 (is zero, function allocates buffer itself) |
| void zb_secur_setup_nwk_key | ( | zb_uint8_t * | key, |
| zb_uint8_t | i | ||
| ) |
Setup NWK key from the application level manually.
| key | - key to be used |
| i | - key number (0-3) |
Call this routine at TC to change random nwk key generated from zb_ib_set_defaults to well-known key. To be used in certification tests mainly.