Logo
Developing with ZBOSS for Zigbee
Configure reporting command sending and parsing

Data Structures

struct  zb_zcl_configure_reporting_req_clnt_s
 
struct  zb_zcl_configure_reporting_req_srv_s
 
union  zb_zcl_configure_reporting_req_u_s
 General type for Configure Reporting Request command. More...
 
struct  zb_zcl_configure_reporting_req_s
 One chunk of Configure reporting command request. More...
 
struct  zb_zcl_configure_reporting_res_s
 

Macros

#define ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_REQ(data_buf, config_rep_req)
 Parses Configure reporting command request and returns next Attribute reporting configuration record or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_RES(data_buf, config_rep_res)
 Parses Configure reporting response and returns next configure attribute status record or NULL if there is no more data. More...
 
#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ(buffer, ptr, def_resp)
 Initialize Configure reporting command (report send case) More...
 
#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ_MANUF(buffer, ptr, def_resp, manuf_code)
 Initialize Configure reporting command (report send case) More...
 
#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_CLI_REQ(buffer, ptr, def_resp)
 Initialize Configure reporting command (report receive case) More...
 
#define ZB_ZCL_GENERAL_ADD_SEND_REPORT_CONFIGURE_REPORTING_REQ( ptr, attr_id, attr_type, min_interval, max_interval, report_change)
 Add attribute reporting configuration record to command payload (report send case) More...
 
#define ZB_ZCL_GENERAL_ADD_RECV_REPORT_CONFIGURE_REPORTING_REQ(ptr, attr_id, timeout)
 Add attribute reporting configuration record to command payload (report receive case) More...
 
#define ZB_ZCL_GENERAL_SEND_CONFIGURE_REPORTING_REQ( buffer, ptr, addr, dst_addr_mode, dst_ep, ep, prfl_id, cluster_id, cb)
 Sends Configure reporting command. More...
 

Typedefs

typedef struct zb_zcl_configure_reporting_req_clnt_s zb_zcl_configure_reporting_req_clnt_t
 
typedef struct zb_zcl_configure_reporting_req_srv_s zb_zcl_configure_reporting_req_srv_t
 
typedef union zb_zcl_configure_reporting_req_u_s zb_zcl_configure_reporting_req_u_t
 General type for Configure Reporting Request command. More...
 
typedef struct zb_zcl_configure_reporting_req_s zb_zcl_configure_reporting_req_t
 One chunk of Configure reporting command request. More...
 
typedef enum zb_zcl_configure_reporting_direction_value_e zb_zcl_configure_reporting_direction_value_t
 
typedef struct zb_zcl_configure_reporting_res_s zb_zcl_configure_reporting_res_t
 

Enumerations

enum  zb_zcl_configure_reporting_direction_value_e { ZB_ZCL_CONFIGURE_REPORTING_SEND_REPORT = 0x00, ZB_ZCL_CONFIGURE_REPORTING_RECV_REPORT = 0x01 }
 

Detailed Description

Most of actions related to the attribute reporting configuration are implemented in ZCL internals.

As described in ZCL spec, subclause 2.4.7, Configure Reporting command has two forms:

Request to configure server for attribute reporting can be filled like in the snippet below:

cmd_ptr,
cmd_ptr, ZB_ZCL_ATTR_ON_OFF_ON_OFF_ID, ZB_ZCL_ATTR_TYPE_BOOL, SIMPLE_GW_REPORTING_MIN_INTERVAL,
SIMPLE_GW_REPORTING_MAX_INTERVAL(dev_idx), 0);
ZB_ZCL_GENERAL_SEND_CONFIGURE_REPORTING_REQ(buf, cmd_ptr, g_device_ctx.devices[dev_idx].short_addr, ZB_APS_ADDR_MODE_16_ENDP_PRESENT,
g_device_ctx.devices[dev_idx].endpoint, SIMPLE_GW_ENDPOINT,
ZB_AF_HA_PROFILE_ID, ZB_ZCL_CLUSTER_ID_ON_OFF, configure_reporting_cb);

Other variant of the command can be filled in a similar way with ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_CLI_REQ() and ZB_ZCL_GENERAL_ADD_RECV_REPORT_CONFIGURE_REPORTING_REQ() macros, and scheduled for sending with ZB_ZCL_GENERAL_SEND_CONFIGURE_REPORTING_REQ() macro.

Configure reporting request record can be parsed as:

zb_bufid_t buffer = pointer_to_the_packet_buffer;
...
do
{
if (! req_record)
{
break;
}
process_request_record(req_record);
} while (1);

Configure Reporting response command will be generated automatically by ZCL internals. Response record to the Configure Reporting command can be parsed as:

If there are several Configure Reporting response records, they could be processed cyclically in the same manner as Configure Reporting request ones.

Macro Definition Documentation

§ ZB_ZCL_GENERAL_ADD_RECV_REPORT_CONFIGURE_REPORTING_REQ

#define ZB_ZCL_GENERAL_ADD_RECV_REPORT_CONFIGURE_REPORTING_REQ (   ptr,
  attr_id,
  timeout 
)
Value:
{ \
ZB_ZCL_PACKET_PUT_DATA8(ptr, ZB_ZCL_CONFIGURE_REPORTING_RECV_REPORT); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (attr_id)); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (timeout)); \
}
Definition: zb_zcl_commands.h:1464

Add attribute reporting configuration record to command payload (report receive case)

Parameters
ptr- command buffer pointer
attr_id- attribute identifier
timeout- reporting timeout

§ ZB_ZCL_GENERAL_ADD_SEND_REPORT_CONFIGURE_REPORTING_REQ

#define ZB_ZCL_GENERAL_ADD_SEND_REPORT_CONFIGURE_REPORTING_REQ (   ptr,
  attr_id,
  attr_type,
  min_interval,
  max_interval,
  report_change 
)
Value:
{ \
ZB_ZCL_PACKET_PUT_DATA8(ptr, ZB_ZCL_CONFIGURE_REPORTING_SEND_REPORT); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (attr_id)); \
ZB_ZCL_PACKET_PUT_DATA8(ptr, (attr_type)); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (min_interval)); \
ZB_ZCL_PACKET_PUT_DATA16_VAL(ptr, (max_interval)); \
if (zb_zcl_is_analog_data_type(attr_type)) \
{ \
(ptr) = zb_zcl_put_value_to_packet((ptr), (attr_type), report_change); \
} \
}
Definition: zb_zcl_commands.h:1463
zb_uint8_t * zb_zcl_put_value_to_packet(zb_uint8_t *cmd_ptr, zb_uint8_t attr_type, zb_uint8_t *attr_value)
zb_bool_t zb_zcl_is_analog_data_type(zb_uint8_t attr_type)
Check whether type of ZCL attribute is analog.

Add attribute reporting configuration record to command payload (report send case)

Parameters
ptr- command buffer pointer
attr_id- attribute identifier
attr_type- type of the attribute
min_interval- reporting minimum interval
max_interval- reporting maximum interval
report_change- reportable value change

§ ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_REQ

#define ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_REQ (   data_buf,
  config_rep_req 
)

Parses Configure reporting command request and returns next Attribute reporting configuration record or NULL if there is no more data.

If request contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing Parses Configure reporting command data
config_rep_req- out pointer to zb_zcl_configure_reporting_req_t, containing Attribute reporting configuration record
Note
data_buf buffer should contain Configure reporting command payload, without ZCL header. Each parsed Attribute reporting configuration record is extracted from initial data_buf buffer

§ ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_RES

#define ZB_ZCL_GENERAL_GET_NEXT_CONFIGURE_REPORTING_RES (   data_buf,
  config_rep_res 
)

Parses Configure reporting response and returns next configure attribute status record or NULL if there is no more data.

If response contains invalid data, NULL is returned.

Parameters
data_buf- ID zb_bufid_t of a buffer containing Configure reporting response data
config_rep_res- out pointer to zb_zcl_configure_reporting_res_t, containing Configure attribute status record
Note
data_buf buffer should contain Configure reporting response payload, without ZCL header. Each parsed Configure attribute status record is extracted from initial data_buf buffer

§ ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_CLI_REQ

#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_CLI_REQ (   buffer,
  ptr,
  def_resp 
)
Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_CONFIG_REPORT); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_FRAME_DIRECTION_TO_CLI
Definition: zb_zcl_common.h:1062
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1013
#define ZB_ZCL_CMD_CONFIG_REPORT
Definition: zb_zcl_commands.h:72

Initialize Configure reporting command (report receive case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ

#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ (   buffer,
  ptr,
  def_resp 
)
Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_ZCL_CMD_CONFIG_REPORT); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_FRAME_DIRECTION_TO_SRV
Definition: zb_zcl_common.h:1060
#define ZB_ZCL_NOT_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1013
#define ZB_ZCL_CMD_CONFIG_REPORT
Definition: zb_zcl_commands.h:72

Initialize Configure reporting command (report send case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response

§ ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ_MANUF

#define ZB_ZCL_GENERAL_INIT_CONFIGURE_REPORTING_SRV_REQ_MANUF (   buffer,
  ptr,
  def_resp,
  manuf_code 
)
Value:
{ \
ptr = ZB_ZCL_START_PACKET(buffer); \
ZB_ZCL_CONSTRUCT_GENERAL_COMMAND_REQ_FRAME_CONTROL_A( \
ZB_ZCL_CONSTRUCT_COMMAND_HEADER_EXT(ptr, ZB_ZCL_GET_SEQ_NUM(), ZB_TRUE, \
manuf_code, ZB_ZCL_CMD_CONFIG_REPORT); \
}
#define ZB_ZCL_GET_SEQ_NUM()
Return next sequence number for ZCL frame.
Definition: zb_zcl_common.h:1463
#define ZB_ZCL_START_PACKET(zbbuf)
Initializes zb_buf_t buffer and returns pointer to the beginning of array.
Definition: zb_zcl_common.h:1543
#define ZB_ZCL_FRAME_DIRECTION_TO_SRV
Definition: zb_zcl_common.h:1060
#define ZB_ZCL_MANUFACTURER_SPECIFIC
Definition: zb_zcl_common.h:1016
#define ZB_TRUE
Definition: zb_types.h:350
#define ZB_ZCL_CMD_CONFIG_REPORT
Definition: zb_zcl_commands.h:72

Initialize Configure reporting command (report send case)

Parameters
bufferto put packet to
ptr- command buffer pointer
def_resp- enable/disable default response
manuf_code- manufacturer specific code

§ ZB_ZCL_GENERAL_SEND_CONFIGURE_REPORTING_REQ

#define ZB_ZCL_GENERAL_SEND_CONFIGURE_REPORTING_REQ (   buffer,
  ptr,
  addr,
  dst_addr_mode,
  dst_ep,
  ep,
  prfl_id,
  cluster_id,
  cb 
)
Value:
{ \
ZB_ZCL_FINISH_PACKET(buffer, ptr) \
ZB_ZCL_SEND_COMMAND_SHORT(buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cluster_id, cb); \
}

Sends Configure reporting command.

Parameters
bufferto put data to
ptr- pointer to the memory area to put data to
addr- address to send packet to
dst_addr_mode- addressing mode
dst_ep- destination endpoint
ep- sending endpoint
prfl_id- profile identifier
cluster_id- cluster identifier
cb- callback for getting command send status

Typedef Documentation

§ zb_zcl_configure_reporting_direction_value_t

Configure reporting command, direction field values

§ zb_zcl_configure_reporting_req_clnt_t

u.clnt: as usual, cluster with client role sends this request to a server to configure reporting: how attribute should be reported by a server

§ zb_zcl_configure_reporting_req_srv_t

u.srv: as usual, cluster with server role sends this request to a client, to inform him how an attribute will be reported by a server

§ zb_zcl_configure_reporting_req_t

One chunk of Configure reporting command request.

Attribute reporting configuration record

§ zb_zcl_configure_reporting_req_u_t

§ zb_zcl_configure_reporting_res_t

One chunk of Configure reporting response command

Attribute status record

Enumeration Type Documentation

§ zb_zcl_configure_reporting_direction_value_e

Configure reporting command, direction field values

Enumerator
ZB_ZCL_CONFIGURE_REPORTING_SEND_REPORT 

Report should be send by a cluster.

ZB_ZCL_CONFIGURE_REPORTING_RECV_REPORT 

Report should be received by a cluster.