Macros | |
| #define | ZB_ZCL_CLUSTER_ID_SUBGHZ_SERVER_ROLE_GENERATED_CMD_LIST ZB_ZCL_SUBGHZ_SRV_CMD_SUSPEND_ZCL_MESSAGES |
| #define | ZB_ZCL_CLUSTER_ID_SUBGHZ_CLIENT_ROLE_RECEIVED_CMD_LIST ZB_ZCL_CLUSTER_ID_SUBGHZ_SERVER_ROLE_GENERATED_CMD_LIST |
| #define | ZB_ZCL_CLUSTER_ID_SUBGHZ_CLIENT_ROLE_GENERATED_CMD_LIST ZB_ZCL_SUBGHZ_CLI_CMD_GET_SUSPEND_ZCL_MESSAGES_STATUS |
| #define | ZB_ZCL_CLUSTER_ID_SUBGHZ_SERVER_ROLE_RECEIVED_CMD_LIST ZB_ZCL_CLUSTER_ID_SUBGHZ_CLIENT_ROLE_GENERATED_CMD_LIST |
Typedefs | |
| typedef enum zb_zcl_subghz_srv_cmd_e | zb_zcl_subghz_srv_cmd_t |
| Sub-GHz cluster's server-side commands IDs. More... | |
| typedef zb_uint8_t | zb_zcl_subghz_suspend_zcl_msg_payload_t |
| SuspendZCLMessages command payload More... | |
| typedef enum zb_zcl_subghz_cli_cmd_e | zb_zcl_subghz_cli_cmd_t |
| Sub-GHz cluster's cliend-side commands IDs. More... | |
Enumerations | |
| enum | zb_zcl_subghz_srv_cmd_e { ZB_ZCL_SUBGHZ_SRV_CMD_SUSPEND_ZCL_MESSAGES = 0x00 } |
| Sub-GHz cluster's server-side commands IDs. More... | |
| enum | zb_zcl_subghz_cli_cmd_e { ZB_ZCL_SUBGHZ_CLI_CMD_GET_SUSPEND_ZCL_MESSAGES_STATUS = 0x00 } |
| Sub-GHz cluster's cliend-side commands IDs. More... | |
| typedef enum zb_zcl_subghz_cli_cmd_e zb_zcl_subghz_cli_cmd_t |
Sub-GHz cluster's cliend-side commands IDs.
| typedef enum zb_zcl_subghz_srv_cmd_e zb_zcl_subghz_srv_cmd_t |
Sub-GHz cluster's server-side commands IDs.
SuspendZCLMessages command payload
An unsigned 8-bit integer indicating the period, in minutes, during which ZCL communications from the device shall be suspended. A value of zero shall indicate that ZCL communications are not currently suspended.
Sub-GHz cluster's cliend-side commands IDs.
Sub-GHz cluster's server-side commands IDs.