Data Structures | |
| struct | zb_zcl_ota_upgrade_file_header_s |
| Structure representation of OTA File Header, see ZCL8 specification, subsection 11.4.2, Table 11-2. OTA Header Fields. More... | |
| struct | zb_zcl_ota_upgrade_file_header_optional_s |
| struct | zb_zcl_ota_upgrade_sub_element_s |
| Structure representation of OTA File Sub-element, see ZCL8 specification, subsection 11.4.3. More... | |
| struct | zb_zcl_ota_upgrade_ecdsa_s |
| Structure representation of OTA ECDSA Signature (Crypto Suite 1), see ZCL8 specification, subsection 11.4.6. More... | |
| struct | zb_zcl_ota_upgrade_ecdsa_signing_s |
| Structure representation of OTA ECDSA Signature, see OTA spec 6.3.6. More... | |
| struct | zb_zcl_ota_upgrade_ecdsa_certificate_s |
| Structure representation of OTA ECDSA Certificate, see OTA spec 6.3.7. More... | |
| struct | zb_zcl_ota_upgrade_server_insert_file_s |
| Structure representation of Data for insert OTA file to upgrade mechanism. More... | |
| struct | zb_zcl_ota_upgrade_server_remove_file_s |
| Structure representation of Data for insert OTA file to upgrade mechanism. More... | |
| struct | zb_zcl_ota_upgrade_data_s |
| Structure representation of OTA file on server side. More... | |
| struct | zb_zcl_ota_upgrade_server_variable_s |
| Structure representation of server side variables. More... | |
| struct | zb_zcl_ota_upgrade_srv_query_img_param_s |
| struct | zb_zcl_ota_upgrade_srv_upgrade_started_param_s |
| struct | zb_zcl_ota_upgrade_srv_upgrade_aborted_param_s |
| struct | zb_zcl_ota_upgrade_srv_upgrade_end_param_s |
| struct | zb_zcl_ota_upgrade_client_variable_s |
| Structure representation of client side variables. More... | |
| struct | zb_zcl_ota_upgrade_attrs_s |
| OTA Upgrade cluster attributes structure. More... | |
| struct | zb_zcl_ota_upgrade_query_next_image_s |
| Structure representation of Query Next Image Request command payload. More... | |
| struct | zb_zcl_ota_upgrade_image_block_s |
| Structure representation of Image Block Request command payload. More... | |
| struct | zb_zcl_ota_upgrade_image_page_s |
| Structure representation of Image Page Request command payload. More... | |
| struct | zb_zcl_ota_upgrade_upgrade_end_s |
| Structure representation of Upgrade End Request command payload. More... | |
| struct | zb_zcl_ota_upgrade_query_specific_file_s |
| Structure representation of Query Specific File Request command payload. More... | |
| struct | zb_zcl_ota_upgrade_image_notify_s |
| Structure representation of Image Notify response command payload. More... | |
| struct | zb_zcl_ota_upgrade_query_next_image_res_s |
| Structure representation of Query Next Image Response command payload. More... | |
| struct | zb_zcl_ota_upgrade_image_block_res_s |
| Structure representation of Image Block Response command payload. More... | |
| struct | zb_zcl_ota_upgrade_upgrade_end_res_s |
| Structure representation of Upgrade End Response command payload. More... | |
| struct | zb_zcl_ota_upgrade_query_specific_file_res_s |
| Structure representation of Query Specific File Response command payload. More... | |
| struct | zb_zcl_ota_upgrade_value_param_s |
| Declare User Application about upgrade status. More... | |
Typedefs | |
| typedef struct zb_zcl_ota_upgrade_value_param_s | zb_zcl_ota_upgrade_value_param_t |
| Declare User Application about upgrade status. | |
Enumerations | |
| enum | zb_zcl_ota_upgrade_status_e { ZB_ZCL_OTA_UPGRADE_STATUS_START, ZB_ZCL_OTA_UPGRADE_STATUS_APPLY, ZB_ZCL_OTA_UPGRADE_STATUS_RECEIVE, ZB_ZCL_OTA_UPGRADE_STATUS_FINISH, ZB_ZCL_OTA_UPGRADE_STATUS_ABORT, ZB_ZCL_OTA_UPGRADE_STATUS_CHECK, ZB_ZCL_OTA_UPGRADE_STATUS_OK, ZB_ZCL_OTA_UPGRADE_STATUS_ERROR, ZB_ZCL_OTA_UPGRADE_STATUS_REQUIRE_MORE_IMAGE, ZB_ZCL_OTA_UPGRADE_STATUS_BUSY, ZB_ZCL_OTA_UPGRADE_STATUS_SERVER_NOT_FOUND } |
| Possible statuses of OTA upgrade. | |
Functions | |
| zb_ret_t | zb_zcl_check_value_ota_upgrade (zb_uint16_t attr_id, zb_uint8_t endpoint, zb_uint8_t *value) |
| void | zcl_ota_abort (zb_uint8_t endpoint, zb_uint8_t param) |
| Abort OTA Upgrade process. More... | |
OTA File Header format | |
Hook on Write attribute send Check-in if change Check-in interval & Check-in remain time > new check-in interval Structures for representation OTA File Header | |
| enum | zb_zcl_ota_upgrade_file_header_fc_e { ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FC_CREDENTIAL_VER = 1 << 0, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FC_DEVICE_SPECIFIC = 1 << 1, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FC_HW_VER = 1 << 2 } |
| OTA File header - fc fields structure. More... | |
| enum | zb_zcl_ota_upgrade_file_header_image_type_e { ZB_ZCL_OTA_UPGRADE_FILE_HEADER_IMAGE_MANUF_SPEC_MAX = 0xffbf, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_IMAGE_SECURITY_CRED = 0xffc0, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_IMAGE_CONFIG = 0xffc1, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_IMAGE_LOG = 0xffc2, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_IMAGE_WILD_CARD = 0xffff } |
| OTA File header - Image Type Values. More... | |
| enum | zb_zcl_ota_upgrade_file_header_stack_version_e { ZB_ZCL_OTA_UPGRADE_FILE_HEADER_STACK_2006 = 0x0000, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_STACK_2007 = 0x0001, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_STACK_PRO = 0x0002, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_STACK_IP = 0x0003 } |
| OTA File header - Zigbee Stack version. More... | |
| enum | zb_zcl_ota_upgrade_file_header_security_version_e { ZB_ZCL_OTA_UPGRADE_FILE_HEADER_SECURITY_VER_SE1_0 = 0x00, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_SECURITY_VER_SE1_1 = 0x01, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_SECURITY_VER_SE2_0 = 0x02, ZB_ZCL_OTA_UPGRADE_FILE_HEADER_SECURITY_VER_SE1_2 = 0x03 } |
| OTA File header - Security Credential Version. More... | |
| typedef struct zb_zcl_ota_upgrade_file_header_s | zb_zcl_ota_upgrade_file_header_t |
| Structure representation of OTA File Header, see ZCL8 specification, subsection 11.4.2, Table 11-2. OTA Header Fields. | |
| typedef struct zb_zcl_ota_upgrade_file_header_optional_s | zb_zcl_ota_upgrade_file_header_optional_t |
| #define | ZB_ZCL_OTA_FILE_IS_FILE_SPECIFIC(head) (((head)->fc) & ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FC_DEVICE_SPECIFIC) |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FILE_ID 0x0BEEF11E |
| Default OTA Upgrade File Identifier, see ZCL8 specification, subsection 11.4.2.1. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_HEADER_FILE_VERSION 0x0100 |
| Default OTA Upgrade File Version, see ZCL8 specification, subsection 11.4.2.2. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_HEADER_MANUFACTURE_CODE_WILD_CARD 0xffff |
| Special Manufacturer Code, see ZCL8 specification, subsection 11.4.2.5. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_APP_RELEASE(ver) (((ver) >>24) & 0xff) |
| OTA Upgrade File Version, App release, see ZCL8 specification, subsection 11.4.2.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_APP_BUILD(ver) (((ver) >>16) & 0xff) |
| OTA Upgrade File Version, App build, see ZCL8 specification, subsection 11.4.2.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_STACK_RELEASE(ver) (((ver) >>8) & 0xff) |
| OTA Upgrade File Version, Stack release, see ZCL8 specification, subsection 11.4.2.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_STACK_BUILD(ver) ((ver) & 0xff) |
| OTA Upgrade File Version, Stack build, see ZCL8 specification, subsection 11.4.2.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_MAKE_VERSION(app_rel, app_build, stack_rel, stack_build) ((app_rel) << 24 | (app_build) << 16 | (stack_rel) << 8 | (stack_build)) |
| OTA Upgrade File Version, make file version, see ZCL8 specification, subsection 11.4.2.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_VERSION_CMP(ver1, ver2) ( (ver1) != (ver2) ) |
| Compare 2 OTA versions and decide if it is needed to do upgrade. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_HW_VERSION(ver) (((ver) >>8) & 0xff) |
| OTA Upgrade HW Version Get Version, see ZCL8 specification, subsection 11.4.2.13. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_GET_HW_REVISION(ver) ((ver) & 0xff) |
| OTA Upgrade HW Version Get Revision, see ZCL8 specification, subsection 11.4.2.13. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_MAKE_HW_VERSION(ver, rev) ((ver) << 8 | (rev)) |
| OTA Upgrade Make HW Version, see ZCL8 specification, subsection 11.4.2.13. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_HW_VERSION_DEF_VALUE 0xffff |
| Default value of OTA Upgrade HW Version. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_DEST_ADDRESS_DEF_VALUE { 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff } |
| Default value of OTA Upgrade destination address. | |
OTA File Sub-element format | |
| enum | zb_zcl_ota_upgrade_sub_element_tags_e { ZB_ZCL_OTA_UPGRADE_FILE_TAG_UPGRADE_IMAGE = 0x0000, ZB_ZCL_OTA_UPGRADE_FILE_TAG_ECDSA = 0x0001, ZB_ZCL_OTA_UPGRADE_FILE_TAG_ECDSA_CERT = 0x0002, ZB_ZCL_OTA_UPGRADE_FILE_TAG_IMAGE_INTEGRITY_CODE = 0x0003, ZB_ZCL_OTA_UPGRADE_FILE_TAG_PICTURE_DATA = 0x0004, ZB_ZCL_OTA_UPGRADE_FILE_TAG_ECDSA_V_2 = 0x0005, ZB_ZCL_OTA_UPGRADE_FILE_TAG_ECDSA_CERT_V_2 = 0x0006, ZB_ZCL_OTA_UPGRADE_FILE_TAG_MANUF_MIN = 0xf000, ZB_ZCL_OTA_UPGRADE_FILE_TAG_MANUF_MAX = 0xffff } |
| OTA File header - Tag Identifiers. More... | |
| typedef struct zb_zcl_ota_upgrade_sub_element_s | zb_zcl_ota_upgrade_sub_element_t |
| Structure representation of OTA File Sub-element, see ZCL8 specification, subsection 11.4.3. | |
| typedef struct zb_zcl_ota_upgrade_ecdsa_s | zb_zcl_ota_upgrade_ecdsa_t |
| Structure representation of OTA ECDSA Signature (Crypto Suite 1), see ZCL8 specification, subsection 11.4.6. | |
| typedef struct zb_zcl_ota_upgrade_ecdsa_signing_s | zb_zcl_ota_upgrade_ecdsa_signing_t |
| Structure representation of OTA ECDSA Signature, see OTA spec 6.3.6. | |
| typedef struct zb_zcl_ota_upgrade_ecdsa_certificate_s | zb_zcl_ota_upgrade_ecdsa_ertificate_t |
| Structure representation of OTA ECDSA Certificate, see OTA spec 6.3.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_TAG_ID ZB_ZCL_OTA_UPGRADE_FILE_TAG_ECDSA |
| Special Manufacturer Code, see ZCL8 specification, subsection 11.4.6. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_LENGTH 0x00000032 |
| Special Manufacturer Code, see ZCL8 specification, subsection 11.4.6. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_SIGNING_TAG_ID 0x0002 |
| Special Manufacturer Code, see spec 6.3.6. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_SIGNING_LENGTH 0x00000030 |
| Special Manufacturer Code, see spec 6.3.6. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_CERTIFICATE_TAG_ID 0x0003 |
| Special Manufacturer Code, see spec 6.3.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_ECDSA_CERTIFICATE_LENGTH 0x00000010 |
| Special Manufacturer Code, see spec 6.3.7. | |
OTA Upgrade cluster attributes | |
| enum | zb_zcl_ota_upgrade_attr_e { ZB_ZCL_ATTR_OTA_UPGRADE_SERVER_ID = 0x0000, ZB_ZCL_ATTR_OTA_UPGRADE_FILE_OFFSET_ID = 0x0001, ZB_ZCL_ATTR_OTA_UPGRADE_FILE_VERSION_ID = 0x0002, ZB_ZCL_ATTR_OTA_UPGRADE_STACK_VERSION_ID = 0x0003, ZB_ZCL_ATTR_OTA_UPGRADE_DOWNLOADED_FILE_VERSION_ID = 0x0004, ZB_ZCL_ATTR_OTA_UPGRADE_DOWNLOADED_STACK_VERSION_ID = 0x0005, ZB_ZCL_ATTR_OTA_UPGRADE_IMAGE_STATUS_ID = 0x0006, ZB_ZCL_ATTR_OTA_UPGRADE_MANUFACTURE_ID = 0x0007, ZB_ZCL_ATTR_OTA_UPGRADE_IMAGE_TYPE_ID = 0x0008, ZB_ZCL_ATTR_OTA_UPGRADE_MIN_BLOCK_REQUE_ID = 0x0009, ZB_ZCL_ATTR_OTA_UPGRADE_IMAGE_STAMP_ID = 0x000a, ZB_ZCL_ATTR_OTA_UPGRADE_UPGRADE_ACTIVATION_POLICY_ID = 0x000b, ZB_ZCL_ATTR_OTA_UPGRADE_UPGRADE_TIMEOUT_POLICY_ID = 0x000c, ZB_ZCL_ATTR_OTA_UPGRADE_SERVER_ENDPOINT_ID = 0xfff3, ZB_ZCL_ATTR_OTA_UPGRADE_SERVER_ADDR_ID = 0xfff2, ZB_ZCL_ATTR_OTA_UPGRADE_CLIENT_DATA_ID = 0xfff1, ZB_ZCL_ATTR_OTA_UPGRADE_SERVER_DATA_ID = 0xfff0 } |
| OTA Upgrade cluster attribute identifiers. More... | |
| enum | zb_zcl_ota_upgrade_image_status_e { ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_NORMAL = 0x00, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_DOWNLOADING = 0x01, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_DOWNLOADED = 0x02, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_WAITING_UPGRADE = 0x03, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_COUNT_DOWN = 0x04, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_WAIT_FOR_MORE = 0x05, ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_WAIT_TO_UPGRADE_VIA_EXT_EVENT = 0x06 } |
| OTA Image Upgrade Status Attribute Values. More... | |
| typedef zb_ret_t(* | zb_zcl_ota_upgrade_next_data_ind_t) (zb_uint8_t index, zb_zcl_parsed_hdr_t *zcl_header, zb_uint32_t offset, zb_uint8_t size, zb_uint8_t **data) |
| Callback function for send next data portion. More... | |
| typedef struct zb_zcl_ota_upgrade_server_insert_file_s | zb_zcl_ota_upgrade_server_insert_file_t |
| Structure representation of Data for insert OTA file to upgrade mechanism. | |
| typedef struct zb_zcl_ota_upgrade_server_remove_file_s | zb_zcl_ota_upgrade_server_remove_file_t |
| Structure representation of Data for insert OTA file to upgrade mechanism. | |
| typedef struct zb_zcl_ota_upgrade_data_s | zb_zcl_ota_upgrade_data_t |
| Structure representation of OTA file on server side. | |
| typedef struct zb_zcl_ota_upgrade_server_variable_s | zb_zcl_ota_upgrade_server_variable_t |
| Structure representation of server side variables. | |
| typedef struct zb_zcl_ota_upgrade_srv_query_img_param_s | zb_zcl_ota_upgrade_srv_query_img_param_t |
| typedef struct zb_zcl_ota_upgrade_srv_upgrade_started_param_s | zb_zcl_ota_upgrade_srv_upgrade_started_param_t |
| typedef struct zb_zcl_ota_upgrade_srv_upgrade_aborted_param_s | zb_zcl_ota_upgrade_srv_upgrade_aborted_param_t |
| typedef struct zb_zcl_ota_upgrade_srv_upgrade_end_param_s | zb_zcl_ota_upgrade_srv_upgrade_end_param_t |
| typedef struct zb_zcl_ota_upgrade_client_variable_s | zb_zcl_ota_upgrade_client_variable_t |
| Structure representation of client side variables. | |
| typedef struct zb_zcl_ota_upgrade_attrs_s | zb_zcl_ota_upgrade_attrs_t |
| OTA Upgrade cluster attributes structure. | |
| void | zb_zcl_ota_upgrade_init_server (zb_uint8_t endpoint, zb_zcl_ota_upgrade_next_data_ind_t next_data_ind_cb) |
| Initialize OTA Upgrade cluster - server part For server clear custom data and registry next data indication. More... | |
| zb_ret_t | zb_zcl_ota_upgrade_insert_file (zb_uint8_t param) |
| Insert upgrade OTA file into Server upgrade table. More... | |
| zb_ret_t | zb_zcl_ota_upgrade_remove_file (zb_uint8_t param) |
| Remove upgrade file from Server upgrade table. More... | |
| void | zb_zcl_ota_upgrade_init_client (zb_uint8_t param) |
| Initialize OTA Upgrade cluster - client part For server clear custom data For client initiate search Upgrade server. More... | |
| zb_ret_t | zb_zcl_ota_upgrade_start_client (zb_uint8_t server_ep, zb_uint16_t server_addr) |
| Start OTA Upgrade client with pre-defined OTA Upgrade Server attributes (without Service Discovery) More... | |
| void | zb_zcl_ota_upgrade_stop_client (void) |
| Stop process OTA Upgrade / OTA query new images Client stop schedule OTA command & clear OTA status. | |
| void | zb_zcl_ota_upgrade_resume_client (zb_uint8_t param, zb_uint8_t upgrade_status) |
| Resume process OTA Upgrade if it was previously suspended by the application. More... | |
| void | zb_zcl_ota_upgrade_set_query_interval (zb_uint8_t endpoint, zb_uint16_t interval) |
| Set Frequency request server about new upgrade file (minutes) More... | |
| void | zb_zcl_ota_upgrade_file_upgraded (zb_uint8_t endpoint) |
| Clear attribute after upgrade. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0004u) |
| Default value for OTA Upgrade cluster revision global attribute. | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_IMAGE_BLOCK_DATA_SIZE_MAX 64 |
| Maximum size data for Query Image Block Request. | |
| #define | ZB_ZCL_OTA_UPGRADE_INSERT_FILE(buf, ep, i, file, upgrade_tm, notify, ret_code) |
| #define | ZB_ZCL_OTA_UPGRADE_REMOVE_FILE(buf, ep, i, ret_code) |
| #define | ZB_ZCL_OTA_UPGRADE_DATA_SIZE_DEF_VALUE 0xff |
| Default value for DataSize, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_JITTER_MIN_VALUE 0x01 |
| Minimum value for QueryJitter, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_JITTER_MAX_VALUE 0x64 |
| Maximum value for QueryJitter, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_JITTER_DEF_VALUE 0x32 |
| Default value for QueryJitter, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_CURRENT_TIME_DEF_VALUE 0xffffffff |
| Default value for currentTime, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_UPGRADE_TIME_DEF_VALUE 0xffffffff |
| Default value for UpgradeTime, OTA spec. | |
| #define | ZB_ZCL_OTA_UPGRADE_SERVER_DEF_VALUE { 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff } |
| Default value for UpgradeServerID attribute, ZCL8 specification, subsection 11.10.1. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_OFFSET_DEF_VALUE 0xffffffff |
| Default value for FileOffset attribute, ZCL8 specification, subsection 11.10.2. | |
| #define | ZB_ZCL_OTA_UPGRADE_FILE_VERSION_DEF_VALUE 0xffffffff |
| Default value for CurrentFileVersion attribute, ZCL8 specification, subsection 11.10.3. | |
| #define | ZB_ZCL_OTA_UPGRADE_STACK_VERSION_DEF_VALUE 0xffff |
| Default value for CurrentZigbeeStackVersion attribute, ZCL8 specification, subsection 11.10.4. | |
| #define | ZB_ZCL_OTA_UPGRADE_DOWNLOADED_FILE_VERSION_DEF_VALUE 0xffffffff |
| Default value for DownloadedFileVersion attribute, ZCL8 specification, subsection 11.10.5. | |
| #define | ZB_ZCL_OTA_UPGRADE_DOWNLOADED_STACK_DEF_VALUE 0xffff |
| Default value for DownloadedZigbeeStackVersion attribute, ZCL8 specification, subsection 11.10.6. | |
| #define | ZB_ZCL_OTA_UPGRADE_IMAGE_STATUS_DEF_VALUE 0x00 |
| Default value for ImageUpgradeStatus attribute, ZCL8 specification, subsection 11.10.7. | |
| #define | ZB_ZCL_OTA_UPGRADE_IMAGE_STAMP_MIN_VALUE 0xfffe |
| Maximum value for MinimumBlockPeriod attribute, ZCL8 specification, subsection 11.10.10. | |
| #define | ZB_ZCL_OTA_UPGRADE_SERVER_ENDPOINT_DEF_VALUE 0xff |
| Default value for OTA server endpoint custom attribute. | |
| #define | ZB_ZCL_OTA_UPGRADE_SERVER_ADDR_DEF_VALUE 0xffff |
| Default value for OTA server addr custom attribute. | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_TIMER_COUNT_DEF (24*60) |
| Default Frequency request server about new upgrade file (minutes) | |
| #define | ZB_ZCL_OTA_UPGRADE_QUERY_TIMER_INTERVAL 60l * ZB_TIME_ONE_SECOND |
| Timer interval for Query timer. | |
| #define | ZB_ZCL_OTA_UPGRADE_MAX_INTERVAL 60 |
| Maximum value of nextImageQuery interval. | |
| #define | ZB_ZCL_OTA_UPGRADE_RESEND_BUFFER_DELAY ZB_TIME_ONE_SECOND * 45 |
| Resend buffer delay. | |
| #define | ZB_ZCL_DECLARE_OTA_UPGRADE_ATTRIB_LIST(attr_list, upgrade_server, file_offset, file_version, stack_version, downloaded_file_ver, downloaded_stack_ver, image_status, manufacturer, image_type, min_block_reque, image_stamp, server_addr, server_ep, hardware_version, max_data_size, query_timer) |
| Declare attribute list for OTA Upgrade cluster - client side. More... | |
| #define | ZB_ZCL_DECLARE_OTA_UPGRADE_ATTR_LIST(attr_list, attrs) |
| Declare attribute list for OTA upgrade cluster (using structure) More... | |
| #define | ZB_ZCL_DECLARE_OTA_UPGRADE_ATTRIB_LIST_SERVER(attr_list, query_jitter, current_time, length) |
| Declare attribute list for OTA Upgrade cluster - server side. More... | |
OTA Upgrade cluster commands | |
| enum | zb_zcl_ota_upgrade_cmd_e { ZB_ZCL_CMD_OTA_UPGRADE_QUERY_NEXT_IMAGE_ID = 0x01, ZB_ZCL_CMD_OTA_UPGRADE_IMAGE_BLOCK_ID = 0x03, ZB_ZCL_CMD_OTA_UPGRADE_IMAGE_PAGE_ID = 0x04, ZB_ZCL_CMD_OTA_UPGRADE_UPGRADE_END_ID = 0x06, ZB_ZCL_CMD_OTA_UPGRADE_QUERY_SPECIFIC_FILE_ID = 0x08 } |
| OTA Upgrade cluster client to server command identifiers. More... | |
| enum | zb_zcl_ota_upgrade_resp_cmd_e { ZB_ZCL_CMD_OTA_UPGRADE_IMAGE_NOTIFY_ID = 0x00, ZB_ZCL_CMD_OTA_UPGRADE_QUERY_NEXT_IMAGE_RESP_ID = 0x02, ZB_ZCL_CMD_OTA_UPGRADE_IMAGE_BLOCK_RESP_ID = 0x05, ZB_ZCL_CMD_OTA_UPGRADE_UPGRADE_END_RESP_ID = 0x07, ZB_ZCL_CMD_OTA_UPGRADE_QUERY_SPECIFIC_FILE_RESP_ID = 0x09, ZB_ZCL_CMD_OTA_UPGRADE_INTERNAL_ABORT_ID = 0xf9 } |
| OTA Upgrade cluster server to client command identifiers. More... | |
| enum | zb_zcl_ota_upgrade_query_next_image_fc_e { ZB_ZCL_OTA_UPGRADE_QUERY_NEXT_IMAGE_HW_VERSION = 1 << 0 } |
| OTA Image Upgrade Status Attribute Values. More... | |
| enum | zb_zcl_ota_upgrade_image_block_fc_e { ZB_ZCL_OTA_UPGRADE_QUERY_IMAGE_BLOCK_IEEE_PRESENT = 1 << 0, ZB_ZCL_OTA_UPGRADE_QUERY_IMAGE_BLOCK_DELAY_PRESENT = 1 << 1 } |
| OTA Image Upgrade Status Attribute Values. More... | |
| enum | zb_zcl_ota_upgrade_image_page_fc_e { ZB_ZCL_OTA_UPGRADE_QUERY_IMAGE_PAGE_IEEE_PRESENT = 1 << 0 } |
| OTA Image Upgrade Status Attribute Values. More... | |
| enum | zb_zcl_ota_upgrade_image_notify_payload_type_e { ZB_ZCL_OTA_UPGRADE_IMAGE_NOTIFY_PAYLOAD_JITTER = 0x00, ZB_ZCL_OTA_UPGRADE_IMAGE_NOTIFY_PAYLOAD_JITTER_CODE = 0x01, ZB_ZCL_OTA_UPGRADE_IMAGE_NOTIFY_PAYLOAD_JITTER_CODE_IMAGE = 0x02, ZB_ZCL_OTA_UPGRADE_IMAGE_NOTIFY_PAYLOAD_JITTER_CODE_IMAGE_VER = 0x03 } |
| OTA Image Upgrade Status Attribute Values. More... | |
| typedef struct zb_zcl_ota_upgrade_query_next_image_s | zb_zcl_ota_upgrade_query_next_image_t |
| Structure representation of Query Next Image Request command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_image_block_s | zb_zcl_ota_upgrade_image_block_t |
| Structure representation of Image Block Request command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_image_page_s | zb_zcl_ota_upgrade_image_page_t |
| Structure representation of Image Page Request command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_upgrade_end_s | zb_zcl_ota_upgrade_upgrade_end_t |
| Structure representation of Upgrade End Request command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_query_specific_file_s | zb_zcl_ota_upgrade_query_specific_file_t |
| Structure representation of Query Specific File Request command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_image_notify_s | zb_zcl_ota_upgrade_image_notify_t |
| Structure representation of Image Notify response command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_query_next_image_res_s | zb_zcl_ota_upgrade_query_next_image_res_t |
| Structure representation of Query Next Image Response command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_image_block_res_s | zb_zcl_ota_upgrade_image_block_res_t |
| Structure representation of Image Block Response command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_upgrade_end_res_s | zb_zcl_ota_upgrade_upgrade_end_res_t |
| Structure representation of Upgrade End Response command payload. More... | |
| typedef struct zb_zcl_ota_upgrade_query_specific_file_res_s | zb_zcl_ota_upgrade_query_specific_file_res_t |
| Structure representation of Query Specific File Response command payload. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_QUERY_NEXT_IMAGE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, fc, manufacturer, image_type, file_version, hw_version, aps_secured) |
| Send "Query Next Image Request" command, see ZCL8 specification, subsection 11.13.4. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_QUERY_NEXT_IMAGE_REQ(data_ptr, buffer, status) |
| Macro for getting "Query Next Image Request" command, see ZCL8 specification, subsection 11.13.4. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, fc, manufacturer, image_type, file_version, file_offset, data_size_max, node_addr, block_delay, current_delay) |
| Send "Image Block Request" command, see ZCL8 specification, subsection 11.13.6. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_IMAGE_BLOCK_REQ(data_ptr, buffer, status) |
| Macro for getting "Image Block Request" command, see ZCL8 specification, subsection 11.13.6. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_PAGE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, fc, manufacturer, image_type, file_version, file_offset, data_size_max, page_size, response_spacing, node_addr) |
| Send "Image Page Request" command, see ZCL8 specification, subsection 11.13.7. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_IMAGE_PAGE_REQ(data_ptr, buffer, status) |
| Macro for getting "Image Page Request" command, see ZCL8 specification, subsection 11.13.7. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_UPGRADE_END_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, status, manufacturer, image_type, file_version) |
| Send "Upgrade End Request" command, see ZCL8 specification, subsection 11.13.9. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_UPGRADE_END_REQ(data_ptr, buffer, status_) |
| Macro for getting "Upgrade End Request" command, see ZCL8 specification, subsection 11.13.9. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_QUERY_SPECIFIC_FILE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, node_addr, manufacturer, image_type, file_version, stack_version) |
| Send "Query Specific File Request" command, see ZCL8 specification, subsection 11.13.10. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_QUERY_SPECIFIC_FILE_REQ(data_ptr, buffer, status) |
| Macro for getting "Query Specific File Request" command, see ZCL8 specification, subsection 11.13.10. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_NOTIFY_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, payload_type, query_jitter, manufacturer, image_type, file_version) |
| Send Image Notify command, see ZCL8 specification, subsection 11.13.3. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_IMAGE_NOTIFY_REQ(data_ptr, buffer, status) |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_QUERY_NEXT_IMAGE_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq, status, manufacturer, image_type, file_version, image_size) |
| Send Query Next Image Response command, see ZCL8 specification, subsection 11.13.5. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_QUERY_NEXT_IMAGE_RES(data_ptr, buffer, status_) |
| Macro for getting Query Next Image Response command, see ZCL8 specification, subsection 11.13.5. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_SUCCESS_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq, manufacturer, image_type, file_version, file_offset, data_size, image_data) |
| Send Image Block Response command - success status, see ZCL8 specification, subsection 11.13.8. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_WAIT_FOR_DATA_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq, current_time, request_time, delay) |
| Send Image Block Response command - wait for data status, see ZCL8 specification, subsection 11.13.8. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_ABORT_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq) |
| Send Image Block Response command - abort status, see ZCL8 specification, subsection 11.13.8. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_IMAGE_BLOCK_RES(data_ptr, buffer, status_) |
| Macro for getting Image Block Response command, see ZCL8 specification, subsection 11.13.8. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_UPGRADE_END_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq, manufacturer, image_type, file_version, current_time, upgrade_time) |
| Send Upgrade End Response command, see ZCL8 specification, subsection 11.13.9.6. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_UPGRADE_END_RES(data_ptr, buffer, status_) |
| Macro for getting Upgrade End Response command, see ZCL8 specification, subsection 11.13.9.6. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_SEND_QUERY_SPECIFIC_FILE_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, seq, status, manufacturer, image_type, file_version, image_size) |
| Send Query Specific File Response command, see ZCL8 specification, subsection 11.13.11. More... | |
| #define | ZB_ZCL_OTA_UPGRADE_GET_QUERY_SPECIFIC_FILE_RES(data_ptr, buffer, status_) |
| Macro for getting Query Specific File Response command, see ZCL8 specification, subsection 11.13.11. More... | |
All commands in the cluster have only request form, and carry no payload.
| #define ZB_ZCL_DECLARE_OTA_UPGRADE_ATTR_LIST | ( | attr_list, | |
| attrs | |||
| ) |
Declare attribute list for OTA upgrade cluster (using structure)
| [in] | attr_list | - attribute list variable name |
| [in] | attrs | - pointer to zb_zcl_ota_upgrade_attrs_s structure |
| #define ZB_ZCL_DECLARE_OTA_UPGRADE_ATTRIB_LIST | ( | attr_list, | |
| upgrade_server, | |||
| file_offset, | |||
| file_version, | |||
| stack_version, | |||
| downloaded_file_ver, | |||
| downloaded_stack_ver, | |||
| image_status, | |||
| manufacturer, | |||
| image_type, | |||
| min_block_reque, | |||
| image_stamp, | |||
| server_addr, | |||
| server_ep, | |||
| hardware_version, | |||
| max_data_size, | |||
| query_timer | |||
| ) |
Declare attribute list for OTA Upgrade cluster - client side.
endcond
| attr_list | - attribute list name |
| upgrade_server | - pointer to variable to store UpgradeServerID attribute |
| file_offset | - pointer to variable to store FileOffset attribute |
| file_version | - pointer to variable to store CurrentFileVersion attribute |
| stack_version | - pointer to variable to store CurrentZigbeeStackVersion attribute |
| downloaded_file_ver | - pointer to variable to store DownloadedFileVersion attribute |
| downloaded_stack_ver | - pointer to variable to store DownloadedZigbeeStackVersion attribute |
| image_status | - pointer to variable to store ImageUpgradeStatus attribute |
| manufacturer | - pointer to variable to store Manufacturer ID attribute |
| image_type | - pointer to variable to store Image Type ID attribute |
| min_block_reque | - pointer to variable to store MinimumBlockReque attribute |
| image_stamp | - pointer to variable to store Image Stamp attribute |
| server_addr | - server short address |
| server_ep | - server endpoint |
| hardware_version | - (const) hardware version |
| max_data_size | - (const) maximum data size Query Block Image commands |
| query_timer | - (const) query timer count |
| #define ZB_ZCL_DECLARE_OTA_UPGRADE_ATTRIB_LIST_SERVER | ( | attr_list, | |
| query_jitter, | |||
| current_time, | |||
| length | |||
| ) |
Declare attribute list for OTA Upgrade cluster - server side.
| attr_list | - attribute list name |
| query_jitter | - (8bit) pointer to variable to store QueryJitter value |
| current_time | - (32bit) pointer to variable to store CurrentTime |
| length | - (const) length of server table with upgrade image data |
| #define ZB_ZCL_OTA_UPGRADE_GET_IMAGE_BLOCK_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Image Block Request" command, see ZCL8 specification, subsection 11.13.6.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_image_block_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_IMAGE_BLOCK_RES | ( | data_ptr, | |
| buffer, | |||
| status_ | |||
| ) |
Macro for getting Image Block Response command, see ZCL8 specification, subsection 11.13.8.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_image_block_res_s. |
| buffer | containing the packet (by pointer). |
| status_ | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_IMAGE_NOTIFY_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
| #define ZB_ZCL_OTA_UPGRADE_GET_IMAGE_PAGE_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Image Page Request" command, see ZCL8 specification, subsection 11.13.7.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_image_page_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_QUERY_NEXT_IMAGE_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Query Next Image Request" command, see ZCL8 specification, subsection 11.13.4.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_query_next_image_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_QUERY_NEXT_IMAGE_RES | ( | data_ptr, | |
| buffer, | |||
| status_ | |||
| ) |
Macro for getting Query Next Image Response command, see ZCL8 specification, subsection 11.13.5.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_query_next_image_res_s. |
| buffer | containing the packet (by pointer). |
| status_ | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_QUERY_SPECIFIC_FILE_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Query Specific File Request" command, see ZCL8 specification, subsection 11.13.10.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_query_specific_file_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_QUERY_SPECIFIC_FILE_RES | ( | data_ptr, | |
| buffer, | |||
| status_ | |||
| ) |
Macro for getting Query Specific File Response command, see ZCL8 specification, subsection 11.13.11.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_query_specific_file_res_s. |
| buffer | containing the packet (by pointer). |
| status_ | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_UPGRADE_END_REQ | ( | data_ptr, | |
| buffer, | |||
| status_ | |||
| ) |
Macro for getting "Upgrade End Request" command, see ZCL8 specification, subsection 11.13.9.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_upgrade_end_s. |
| buffer | containing the packet (by pointer). |
| status_ | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_GET_UPGRADE_END_RES | ( | data_ptr, | |
| buffer, | |||
| status_ | |||
| ) |
Macro for getting Upgrade End Response command, see ZCL8 specification, subsection 11.13.9.6.
| data_ptr | - pointer to a variable of type zb_zcl_ota_upgrade_upgrade_end_res_s. |
| buffer | containing the packet (by pointer). |
| status_ | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_OTA_UPGRADE_INSERT_FILE | ( | buf, | |
| ep, | |||
| i, | |||
| file, | |||
| upgrade_tm, | |||
| notify, | |||
| ret_code | |||
| ) |
| #define ZB_ZCL_OTA_UPGRADE_REMOVE_FILE | ( | buf, | |
| ep, | |||
| i, | |||
| ret_code | |||
| ) |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_ABORT_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq | |||
| ) |
Send Image Block Response command - abort status, see ZCL8 specification, subsection 11.13.8.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| fc, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| file_offset, | |||
| data_size_max, | |||
| node_addr, | |||
| block_delay, | |||
| current_delay | |||
| ) |
Send "Image Block Request" command, see ZCL8 specification, subsection 11.13.6.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| fc | - Field Control, see zb_zcl_ota_upgrade_image_block_fc_e |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| file_offset | - File offset |
| data_size_max | - Maximum data size |
| node_addr | - Request node address |
| block_delay | - BlockRequestDelay |
| current_delay | - Delay current send (millisec) |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_SUCCESS_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| file_offset, | |||
| data_size, | |||
| image_data | |||
| ) |
Send Image Block Response command - success status, see ZCL8 specification, subsection 11.13.8.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| file_offset | - File offset |
| data_size | - data size |
| image_data | - image data |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_BLOCK_WAIT_FOR_DATA_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq, | |||
| current_time, | |||
| request_time, | |||
| delay | |||
| ) |
Send Image Block Response command - wait for data status, see ZCL8 specification, subsection 11.13.8.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| current_time | - Current time |
| request_time | - Request time |
| delay | - BlockRequestDelay |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_NOTIFY_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| payload_type, | |||
| query_jitter, | |||
| manufacturer, | |||
| image_type, | |||
| file_version | |||
| ) |
Send Image Notify command, see ZCL8 specification, subsection 11.13.3.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback for getting command send status |
| payload_type | - Payload type |
| query_jitter | - Query jitter |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| #define ZB_ZCL_OTA_UPGRADE_SEND_IMAGE_PAGE_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| fc, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| file_offset, | |||
| data_size_max, | |||
| page_size, | |||
| response_spacing, | |||
| node_addr | |||
| ) |
Send "Image Page Request" command, see ZCL8 specification, subsection 11.13.7.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| fc | - Field Control, see zb_zcl_ota_upgrade_image_page_fc_e |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| file_offset | - File offset |
| data_size_max | - Maximum data size |
| page_size | - Page size |
| response_spacing | - Response Spacing |
| node_addr | - Request node address |
| #define ZB_ZCL_OTA_UPGRADE_SEND_QUERY_NEXT_IMAGE_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| fc, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| hw_version, | |||
| aps_secured | |||
| ) |
Send "Query Next Image Request" command, see ZCL8 specification, subsection 11.13.4.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| fc | - Field Control, see zb_zcl_ota_upgrade_image_notify_payload_type_e |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| hw_version | - Hardware version |
| aps_secured | - APS security |
| #define ZB_ZCL_OTA_UPGRADE_SEND_QUERY_NEXT_IMAGE_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq, | |||
| status, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| image_size | |||
| ) |
Send Query Next Image Response command, see ZCL8 specification, subsection 11.13.5.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| status | - Status, see zcl_status |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| image_size | - Image size |
| #define ZB_ZCL_OTA_UPGRADE_SEND_QUERY_SPECIFIC_FILE_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| node_addr, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| stack_version | |||
| ) |
Send "Query Specific File Request" command, see ZCL8 specification, subsection 11.13.10.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| node_addr | - Node address |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| stack_version | - Zigbee stack version |
| #define ZB_ZCL_OTA_UPGRADE_SEND_QUERY_SPECIFIC_FILE_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq, | |||
| status, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| image_size | |||
| ) |
Send Query Specific File Response command, see ZCL8 specification, subsection 11.13.11.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| status | - Status, see zcl_status |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| image_size | - Image size |
| #define ZB_ZCL_OTA_UPGRADE_SEND_UPGRADE_END_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| status, | |||
| manufacturer, | |||
| image_type, | |||
| file_version | |||
| ) |
Send "Upgrade End Request" command, see ZCL8 specification, subsection 11.13.9.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| status | - Status, see zcl_status |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| #define ZB_ZCL_OTA_UPGRADE_SEND_UPGRADE_END_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| seq, | |||
| manufacturer, | |||
| image_type, | |||
| file_version, | |||
| current_time, | |||
| upgrade_time | |||
| ) |
Send Upgrade End Response command, see ZCL8 specification, subsection 11.13.9.6.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| seq | - sequence |
| manufacturer | - Manufacturer code |
| image_type | - Image type |
| file_version | - File version |
| current_time | - Current time |
| upgrade_time | - Upgrade time |
Optional parts of the OTA file header See ZCL8 specification, subsection 11.4.2, Table 11-2. OTA Header Fields
Structure representation of Image Block Response command payload.
| typedef struct zb_zcl_ota_upgrade_image_block_s zb_zcl_ota_upgrade_image_block_t |
Structure representation of Image Block Request command payload.
Structure representation of Image Notify response command payload.
| typedef struct zb_zcl_ota_upgrade_image_page_s zb_zcl_ota_upgrade_image_page_t |
Structure representation of Image Page Request command payload.
| typedef zb_ret_t(* zb_zcl_ota_upgrade_next_data_ind_t) (zb_uint8_t index, zb_zcl_parsed_hdr_t *zcl_header, zb_uint32_t offset, zb_uint8_t size, zb_uint8_t **data) |
Callback function for send next data portion.
Structure representation of Query Next Image Response command payload.
Structure representation of Query Next Image Request command payload.
| typedef struct zb_zcl_ota_upgrade_query_specific_file_res_s zb_zcl_ota_upgrade_query_specific_file_res_t |
Structure representation of Query Specific File Response command payload.
Structure representation of Query Specific File Request command payload.
Structure representation of Upgrade End Response command payload.
| typedef struct zb_zcl_ota_upgrade_upgrade_end_s zb_zcl_ota_upgrade_upgrade_end_t |
Structure representation of Upgrade End Request command payload.
OTA Upgrade cluster attribute identifiers.
OTA Upgrade cluster client to server command identifiers.
OTA File header - fc fields structure.
OTA File header - Image Type Values.
OTA File header - Security Credential Version.
OTA File header - Zigbee Stack version.
OTA Image Upgrade Status Attribute Values.
OTA Image Upgrade Status Attribute Values.
OTA Upgrade cluster server to client command identifiers.
OTA File header - Tag Identifiers.
| void zb_zcl_ota_upgrade_file_upgraded | ( | zb_uint8_t | endpoint | ) |
Clear attribute after upgrade.
| endpoint | - endpoint |
| void zb_zcl_ota_upgrade_init_client | ( | zb_uint8_t | param | ) |
Initialize OTA Upgrade cluster - client part For server clear custom data For client initiate search Upgrade server.
| param | - empty buffer |
| void zb_zcl_ota_upgrade_init_server | ( | zb_uint8_t | endpoint, |
| zb_zcl_ota_upgrade_next_data_ind_t | next_data_ind_cb | ||
| ) |
Initialize OTA Upgrade cluster - server part For server clear custom data and registry next data indication.
| endpoint | - destination endpoint |
| next_data_ind_cb | - callback to be called on received image block For client initiate search Upgrade server |
| zb_ret_t zb_zcl_ota_upgrade_insert_file | ( | zb_uint8_t | param | ) |
Insert upgrade OTA file into Server upgrade table.
| param | - buffer with zb_zcl_ota_upgrade_server_insert_file_s structure |
| zb_ret_t zb_zcl_ota_upgrade_remove_file | ( | zb_uint8_t | param | ) |
Remove upgrade file from Server upgrade table.
| param | - buffer with zb_zcl_ota_upgrade_server_remove_file_s structure |
| void zb_zcl_ota_upgrade_resume_client | ( | zb_uint8_t | param, |
| zb_uint8_t | upgrade_status | ||
| ) |
Resume process OTA Upgrade if it was previously suspended by the application.
| param | - buffer to be resumed |
| upgrade_status | - application upgrade status |
| void zb_zcl_ota_upgrade_set_query_interval | ( | zb_uint8_t | endpoint, |
| zb_uint16_t | interval | ||
| ) |
Set Frequency request server about new upgrade file (minutes)
| endpoint | - endpoint of the OTA cluster |
| interval | - new interval value (in minutes) |
| zb_ret_t zb_zcl_ota_upgrade_start_client | ( | zb_uint8_t | server_ep, |
| zb_uint16_t | server_addr | ||
| ) |
Start OTA Upgrade client with pre-defined OTA Upgrade Server attributes (without Service Discovery)
| server_ep | - OTA Upgrade server endpoint |
| server_addr | - OTA Upgrade server short address |
| void zcl_ota_abort | ( | zb_uint8_t | endpoint, |
| zb_uint8_t | param | ||
| ) |
Abort OTA Upgrade process.
| endpoint | - endpoint for OTA Upgrade |
| param | - buffer to be aborted |