Metering cluster client attributes.
| Enumerator |
|---|
| ZB_ZCL_ATTR_METERING_CLI_FUNCTIONAL_NOTIFICATION_FLAGS | FunctionalNotificationFlags attribute is implemented as a set of bit flags which are have a predefined action associated with a bit that is not based on a specific command, but may require the Mirrored device to trigger some additional functionality within the system
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS2 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS3 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS4 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS5 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS6 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS7 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|
| ZB_ZCL_ATTR_METERING_CLI_NOTIFICATION_FLAGS8 | NotificationFlagsN are 32-bit bitmaps that each represent a series of flags. Each flag represents an outstanding command that the Mirror is holding on behalf of the BOMD. Each flag represents a different command. The format of these attributes is dictated by the scheme that is currently in operation.
|