Meter Identification server attributes identifiers.
| Enumerator |
|---|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_COMPANY_NAME | CompanyName is a ZCL Octet String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the UTF-8 format. Company Name defines the meter manufacturer name, decided by manufacturer
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_METER_TYPE_ID | MeterTypeID defines the Meter installation features, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_DATA_QUALITY_ID | DataQualityID defines the Meter Simple Metering information certification type, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_CUSTOMER_NAME | CustomerName is a ZCL Character String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the ASCII format.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_MODEL | Model is a ZCL Octet String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the UTF-8 format. Model defines the meter model name, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_PART_NUMBER | PartNumber is a ZCL Octet String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the UTF-8 format. PartNumber defines the meter part number, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_PRODUCT_REVISION | ProductRevision is a ZCL Octet String field capable of storing up to 6 character string (the first Octet indicates length) encoded in the UTF-8 format. ProductRevision defines the meter revision code, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_SOFTWARE_REVISION | SoftwareRevision is a ZCL Octet String field capable of storing up to 6 character string (the first Octet indicates length) encoded in the UTF-8 format. SoftwareRevision defines the meter software revision code, decided by manufacturer.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_UTILITY_NAME | UtilityName is a ZCL Character String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the ASCII format.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_POD | POD (Point of Delivery) is a ZCL Character String field capable of storing up to 16 character string (the first Octet indicates length) encoded in the ASCII format. POD is the unique identification ID of the premise connection point. It is also a contractual information known by the clients and indicated in the bill.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_AVAILABLE_POWER | AvailablePower represents the InstantaneousDemand that can be distributed to the customer (e.g., 3.3KW power) without any risk of overload. The Available Power SHALL use the same formatting conventions as the one used in the simple metering cluster formatting attribute set for the InstantaneousDemand attribute, i.e., the UnitOfMeasure and DemandFormatting.
|
| ZB_ZCl_ATTR_METER_IDENTIFICATION_POWER_THRESHOLD | PowerThreshold represents a threshold of InstantaneousDemand distributed to the customer (e.g., 4.191KW) that will lead to an imminent risk of overload.
|