Data Structures | |
| struct | zb_zcl_ias_zone_init_test_mode_ha_s |
| Structure representsation of Initiate Test Mode - Errata to 05-3520-29 Spec, 1.1.23.2.2.1. More... | |
| struct | zb_zcl_ias_zone_status_change_not_s |
| Structure representsation of Zone Status Change Notification see ZCL spec 8.2.2.4.1.1. More... | |
| struct | zb_zcl_ias_zone_enroll_request_s |
| Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2. More... | |
| struct | zb_zcl_ias_zone_enroll_res_s |
| Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1. More... | |
| struct | zb_zcl_ias_zone_status_param_s |
| Declare Set/Clear Zone Status bits. More... | |
| struct | zb_zcl_ias_zone_notification_param_s |
| Structure is used to pass parameters for ZoneStatus notification command. More... | |
| struct | zb_zcl_ias_zone_int_ctx_s |
| struct | zb_zcl_ias_zone_enroll_response_value_param_s |
| Declare run Enroll Response command for User Application. More... | |
| struct | zb_zcl_ias_zone_enroll_response_user_app_schedule_e |
Macros | |
| #define | ZB_ZCL_IAS_ZONE_SET_BITS(buffer, ep, set_bits) |
| Set Zone Status bits custom server command. More... | |
| #define | ZB_ZCL_IAS_ZONE_CLEAR_BITS(buffer, ep, set_bits) |
| Clear Zone Status bits custom server command. More... | |
| #define | ZB_ZCL_IAS_ZONE_ENROLL_RESPONSE_SCHEDULE_USER_APP(buffer, pcmd_info, enroll_response_, zone_id_) |
Typedefs | |
| typedef struct zb_zcl_ias_zone_status_param_s | zb_zcl_ias_zone_status_param_t |
| Declare Set/Clear Zone Status bits. | |
| typedef struct zb_zcl_ias_zone_notification_param_s | zb_zcl_ias_zone_notification_param_t |
| Structure is used to pass parameters for ZoneStatus notification command. | |
| typedef zb_ret_t(* | zb_ias_zone_app_callback_t) (zb_uint8_t param, zb_uint16_t general_val) |
| typedef struct zb_zcl_ias_zone_int_ctx_s | zb_zcl_ias_zone_int_ctx_t |
| typedef struct zb_zcl_ias_zone_enroll_response_value_param_s | zb_zcl_ias_zone_enroll_response_value_param_t |
| Declare run Enroll Response command for User Application. | |
| typedef struct zb_zcl_ias_zone_enroll_response_user_app_schedule_e | zb_zcl_ias_zone_enroll_response_user_app_schedule_t |
Enumerations | |
| enum | zb_zcl_general_cb_params_e { ZB_ZCL_VALID_CIE_ADDR_SET = 1, ZB_ZCL_CURR_ZONE_SENSITIVITY_LEVEL_SET = 2, ZB_ZCL_INIT_TEST_MODE = 3, ZB_ZCL_INIT_NORMAL_MODE = 4 } |
Functions | |
| void | zb_zcl_ias_zone_change_status (zb_uint8_t param) |
| zb_bool_t | zb_zcl_ias_zone_set_status (zb_uint8_t ep, zb_uint16_t new_val, zb_uint16_t delay, zb_uint8_t buf_param) |
| Use this function to change IAS Zone status. This function will set new value of ZoneStatus and will send Zone status change notification. More... | |
| void | zb_zcl_ias_zone_register_cb (zb_uint8_t endpoint, zb_callback_t process_result_cb, zb_ias_zone_app_callback_t general_cb) |
| Registry callbacks to get status of Zone Status Change Notification command. More... | |
| zb_bool_t | zb_zcl_ias_zone_check_attr_notify (zb_uint8_t buf_param) |
| checks, if Zone Status change notification should be sent and schedules command if it is needed More... | |
| void | zb_zcl_ias_zone_send_status_change_not (zb_uint8_t param) |
| fills in notification command and sends it | |
| void | zb_zcl_ias_zone_check_cie_addr_on_zcl_initialization (zb_uint8_t ep_id) |
| checks cie address on zcl initialization | |
| zb_ret_t | zb_zcl_ias_zone_put_cie_address_to_binding_whitelist (zb_uint8_t endpoint) |
| puts cie command to binding whitelist table | |
| void | zb_zcl_ias_set_attr_val_post_process (zb_zcl_parsed_hdr_t *cmd_info, zb_uint16_t attr_id, zb_uint8_t *value) |
| IAS Zone specific set attribute value postprocessing. | |
IAS Zone cluster commands | |
| enum | zb_zcl_ias_zone_cmd_e { ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_RESPONSE_ID = 0x00, ZB_ZCL_CMD_IAS_ZONE_INITIATE_NORMAL_OPERATION_MODE_ID = 0x01, ZB_ZCL_CMD_IAS_ZONE_INITIATE_TEST_MODE_ID = 0x02 } |
| IAS Zone cluster command identifiers. More... | |
| enum | zb_zcl_ias_zone_resp_cmd_e { ZB_ZCL_CMD_IAS_ZONE_ZONE_STATUS_CHANGE_NOT_ID = 0x00, ZB_ZCL_CMD_IAS_ZONE_ZONE_ENROLL_REQUEST_ID = 0x01 } |
| IAS Zone cluster response command identifiers. More... | |
| enum | zb_zcl_ias_zone_enroll_responce_code_e { ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_SUCCESS = 0x00, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NOT_SUPPORTED = 0x01, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_NO_ENROLL = 0x02, ZB_ZCL_IAS_ZONE_ENROLL_RESPONCE_CODE_TOO_MANY_ZONES = 0x03 } |
| Values of the Enroll Response Code see ZCL spec 8.2.2.3.1.1. More... | |
| typedef struct zb_zcl_ias_zone_init_test_mode_ha_s | zb_zcl_ias_zone_init_test_mode_t |
| Structure representsation of Initiate Test Mode - Errata to 05-3520-29 Spec, 1.1.23.2.2.1. | |
| typedef struct zb_zcl_ias_zone_status_change_not_s | zb_zcl_ias_zone_status_change_not_t |
| Structure representsation of Zone Status Change Notification see ZCL spec 8.2.2.4.1.1. | |
| typedef struct zb_zcl_ias_zone_enroll_request_s | zb_zcl_ias_zone_enroll_request_t |
| Structure representsation of "Zone Enroll Request" command see ZCL spec 8.2.2.4.1.2. | |
| typedef struct zb_zcl_ias_zone_enroll_res_s | zb_zcl_ias_zone_enroll_res_t |
| Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1. | |
| #define | ZB_ZCL_IAS_ZONE_GET_INITIATE_TEST_MODE_REQ(data_ptr, buffer, status) |
| Macro for getting "Initiate Test Mode" command. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_INITIATE_TEST_MODE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, test_mode_duration, current_zone_sens_level) |
| Initiate Test Mode command. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_INITIATE_NORMAL_OPERATION_MODE_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb) |
| Initiate Normal Operation Mode command. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_STATUS_CHANGE_NOTIFICATION_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, zone_status, extended_status, zone_id, delay) |
| Zone Status Change Notification command. More... | |
| #define | ZB_ZCL_IAS_ZONE_GET_STATUS_CHANGE_NOTIFICATION_REQ(data_ptr, buffer, status) |
| Macro for getting Zone Status Change Notification command. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_REQUEST_REQ( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, cb, zone_type, manufacturer_code) |
| Zone "Zone Enroll Request" command, see ZCL spec 8.2.2.4.2. More... | |
| #define | ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_REQUEST_REQ(data_ptr, buffer, status) |
| Macro for getting Zone Status Change Notification command, see ZCL spec 8.2.2.4.1. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, code, zone_id) |
| Send "Zone Enroll response" command, see ZCL spec 8.2.2.3.1. More... | |
| #define | ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES_EXT( buffer, addr, dst_addr_mode, dst_ep, ep, prfl_id, def_resp, cb, code, zone_id, seq) |
| Send "Zone Enroll response with add parameters - sequency" command, see ZCL spec 8.2.2.3.1. More... | |
| #define | ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_RES(data_ptr, buffer, status) |
| Macro for getting "Zone Enroll response" command. More... | |
IAS Zone cluster definitions
| #define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST | ( | attr_list, | |
| zone_state, | |||
| zone_type, | |||
| zone_status, | |||
| ias_cie_address, | |||
| cie_short_addr, | |||
| cie_ep | |||
| ) |
Declare attribute list for IAS Zone cluster - server side.
| attr_list | - attribute list name |
| zone_state | - pointer to variable to store ZoneState attribute |
| zone_type | - pointer to variable to store ZoneType attribute |
| zone_status | - pointer to variable to store ZoneStatus attribute |
| ias_cie_address | - pointer to variable to store IAS-CIE address attribute |
| cie_short_addr | - custom attribute to store CIE short address |
| cie_ep | - custom attribute to store CIE Endpoint number |
| #define ZB_ZCL_DECLARE_IAS_ZONE_ATTRIB_LIST_EXT | ( | attr_list, | |
| zone_state, | |||
| zone_type, | |||
| zone_status, | |||
| number_of_zone_sens_levels_supported, | |||
| current_zone_sens_level, | |||
| ias_cie_address, | |||
| zone_id, | |||
| cie_short_addr, | |||
| cie_ep | |||
| ) |
Declare attribute list for IAS Zone cluster - server side (extended attribute set)
| attr_list | - attribute list name |
| zone_state | - pointer to variable to store ZoneState attribute |
| zone_type | - pointer to variable to store ZoneType attribute |
| zone_status | - pointer to variable to store ZoneStatus attribute |
| ias_cie_address | - pointer to variable to store IAS-CIE address attribute |
| zone_id | - pointer to variable to store Zone ID attribute |
| number_of_zone_sens_levels_supported | - pointer to variable to store NumberOfZoneSensitivityLevelsSupported attribute |
| current_zone_sens_level | - pointer to variable to store CurrentZoneSensitivityLevel attribute |
| cie_short_addr | - custom attribute to store CIE short address |
| cie_ep | - custom attribute to store CIE Endpoint number |
| #define ZB_ZCL_IAS_ZONE_CLEAR_BITS | ( | buffer, | |
| ep, | |||
| set_bits | |||
| ) |
Clear Zone Status bits custom server command.
| buffer | - to put packet to |
| ep | - sending endpoint |
| set_bits | - flag set of Zone Status, see zb_zcl_ias_zone_zonestatus_e |
| #define ZB_ZCL_IAS_ZONE_ENROLL_RESPONSE_SCHEDULE_USER_APP | ( | buffer, | |
| pcmd_info, | |||
| enroll_response_, | |||
| zone_id_ | |||
| ) |
| #define ZB_ZCL_IAS_ZONE_GET_INITIATE_TEST_MODE_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Initiate Test Mode" command.
| data_ptr | - pointer to a variable of type zb_zcl_ias_zone_init_test_mode_t. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IAS_ZONE_GET_STATUS_CHANGE_NOTIFICATION_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting Zone Status Change Notification command.
| data_ptr | - pointer to a variable of type zb_zcl_ias_zone_status_change_not_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_REQUEST_REQ | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting Zone Status Change Notification command, see ZCL spec 8.2.2.4.1.
| data_ptr | - pointer to a variable of type zb_zcl_ias_zone_enroll_request_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IAS_ZONE_GET_ZONE_ENROLL_RES | ( | data_ptr, | |
| buffer, | |||
| status | |||
| ) |
Macro for getting "Zone Enroll response" command.
| data_ptr | - pointer to a variable of type zb_zcl_ias_zone_enroll_res_s. |
| buffer | containing the packet (by pointer). |
| status | - variable to put parse status to (see zb_zcl_parse_status_t). |
| #define ZB_ZCL_IAS_ZONE_SEND_INITIATE_NORMAL_OPERATION_MODE_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| cb | |||
| ) |
Initiate Normal Operation Mode command.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| cb | - callback for getting command send status |
| #define ZB_ZCL_IAS_ZONE_SEND_INITIATE_TEST_MODE_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| cb, | |||
| test_mode_duration, | |||
| current_zone_sens_level | |||
| ) |
Initiate Test Mode command.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| cb | - callback for getting command send status |
| test_mode_duration | - Test Mode duration |
| current_zone_sens_level | - CurrentZoneSensitivityLevel |
| #define ZB_ZCL_IAS_ZONE_SEND_STATUS_CHANGE_NOTIFICATION_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| cb, | |||
| zone_status, | |||
| extended_status, | |||
| zone_id, | |||
| delay | |||
| ) |
Zone Status Change Notification command.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| cb | - callback for getting command send status |
| zone_status | - Zone Status, see zb_zcl_ias_zone_zonestatus_e |
| extended_status | - Extended Status |
| zone_id | - Zone ID |
| delay | - Delay |
| #define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_REQUEST_REQ | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| cb, | |||
| zone_type, | |||
| manufacturer_code | |||
| ) |
Zone "Zone Enroll Request" command, see ZCL spec 8.2.2.4.2.
| buffer | - to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| cb | - callback for getting command send status |
| zone_type | - Zone Type, see zb_zcl_ias_zone_zonetype_e |
| manufacturer_code | - Manufacture code |
| #define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| code, | |||
| zone_id | |||
| ) |
Send "Zone Enroll response" command, see ZCL spec 8.2.2.3.1.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| code | - Enroll response code, see zb_zcl_ias_zone_enroll_responce_code_e |
| zone_id | - Zone ID |
| #define ZB_ZCL_IAS_ZONE_SEND_ZONE_ENROLL_RES_EXT | ( | buffer, | |
| addr, | |||
| dst_addr_mode, | |||
| dst_ep, | |||
| ep, | |||
| prfl_id, | |||
| def_resp, | |||
| cb, | |||
| code, | |||
| zone_id, | |||
| seq | |||
| ) |
Send "Zone Enroll response with add parameters - sequency" command, see ZCL spec 8.2.2.3.1.
| buffer | to put packet to |
| addr | - address to send packet to |
| dst_addr_mode | - addressing mode |
| dst_ep | - destination endpoint |
| ep | - sending endpoint |
| prfl_id | - profile identifier |
| def_resp | - enable/disable default response |
| cb | - callback |
| code | - Enroll response code, see zb_zcl_ias_zone_enroll_responce_code_e |
| zone_id | - Zone ID |
| seq | - known sequency |
| #define ZB_ZCL_IAS_ZONE_SET_BITS | ( | buffer, | |
| ep, | |||
| set_bits | |||
| ) |
Set Zone Status bits custom server command.
| buffer | - to put packet to |
| ep | - endpoint |
| set_bits | - flag set of Zone Status, see zb_zcl_ias_zone_zonestatus_e |
| typedef struct zb_zcl_ias_zone_enroll_response_user_app_schedule_e zb_zcl_ias_zone_enroll_response_user_app_schedule_t |
Struct for invoke User App & continue after
IAS Zone cluster attribute identifiers.
IAS Zone cluster command identifiers.
Values of the Enroll Response Code see ZCL spec 8.2.2.3.1.1.
IAS Zone cluster response command identifiers.
IAS Zone ZoneStatus attribute flags.
IAS Zone ZoneType value.
| zb_bool_t zb_zcl_ias_zone_check_attr_notify | ( | zb_uint8_t | buf_param | ) |
checks, if Zone Status change notification should be sent and schedules command if it is needed
| void zb_zcl_ias_zone_register_cb | ( | zb_uint8_t | endpoint, |
| zb_callback_t | process_result_cb, | ||
| zb_ias_zone_app_callback_t | general_cb | ||
| ) |
Registry callbacks to get status of Zone Status Change Notification command.
| endpoint | - local endpoint number |
| process_result_cb | - notification sent callback function |
| general_cb | - general callback function |
| zb_bool_t zb_zcl_ias_zone_set_status | ( | zb_uint8_t | ep, |
| zb_uint16_t | new_val, | ||
| zb_uint16_t | delay, | ||
| zb_uint8_t | buf_param | ||
| ) |
Use this function to change IAS Zone status. This function will set new value of ZoneStatus and will send Zone status change notification.
| ep | - local endpoint number |
| new_val | - new value for ZoneStatus |
| delay | - delay in quarter seconds (actual only for HA ZCL version, is ignored for pure ZCL implementation) |
| buf_param | - reference to a buffer that will be used for sending notification. If buffer reference is not specified, notification will NOT be sent |