Logo
Developing with ZBOSS for Zigbee

Macros

#define ZB_ZCL_DRLC_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)
 Default value for DRLC cluster revision global attribute.
 
#define ZB_ZCL_DRLC_CLUSTER_REVISION_MAX   ZB_ZCL_DRLC_CLUSTER_REVISION_DEFAULT
 Maximal value for implemented DRLC cluster revision global attribute.
 

Typedefs

typedef enum zb_zcl_drlc_cli_attr_e zb_zcl_drlc_cli_attr_t
 
typedef enum zb_zcl_drlc_criticality_levels_e zb_zcl_drlc_criticality_levels_t
 
typedef enum zb_zcl_drlc_device_class_e zb_zcl_drlc_device_class_t
 
typedef enum zb_zcl_drlc_event_status_e zb_zcl_drlc_event_status_t
 
typedef enum zb_zcl_drlc_signature_type_e zb_zcl_drlc_signature_type_t
 

Enumerations

enum  zb_zcl_drlc_cli_attr_e { ZB_ZCL_ATTR_DRLC_UTILITY_ENROLLMENT_GROUP = 0x0000, ZB_ZCL_ATTR_DRLC_START_RANDOMIZATION_MINUTES = 0x0001, ZB_ZCL_ATTR_DRLC_DURATION_RANDOMIZATION_MINUTES = 0x0002, ZB_ZCL_ATTR_DRLC_DEVICE_CLASS_VALUE = 0x0003 }
 
enum  zb_zcl_drlc_criticality_levels_e {
  ZB_ZCL_DRLC_CRITICALITY_LEVEL_0 = 0x00, ZB_ZCL_DRLC_CRITICALITY_LEVEL_1, ZB_ZCL_DRLC_CRITICALITY_LEVEL_2, ZB_ZCL_DRLC_CRITICALITY_LEVEL_3,
  ZB_ZCL_DRLC_CRITICALITY_LEVEL_4, ZB_ZCL_DRLC_CRITICALITY_LEVEL_5, ZB_ZCL_DRLC_CRITICALITY_LEVEL_6, ZB_ZCL_DRLC_CRITICALITY_LEVEL_7,
  ZB_ZCL_DRLC_CRITICALITY_LEVEL_8, ZB_ZCL_DRLC_CRITICALITY_LEVEL_9
}
 
enum  zb_zcl_drlc_device_class_e {
  ZB_ZCL_DRLC_DEVICE_CLASS_HVAC = 1 << 0, ZB_ZCL_DRLC_DEVICE_CLASS_STRIP_HEATER = 1 << 1, ZB_ZCL_DRLC_DEVICE_CLASS_WATER_HEATER = 1 << 2, ZB_ZCL_DRLC_DEVICE_CLASS_POOL_PUMP = 1 << 3,
  ZB_ZCL_DRLC_DEVICE_CLASS_SMART_APPLIANCE = 1 << 4, ZB_ZCL_DRLC_DEVICE_CLASS_IRRIGATION_PUMP = 1 << 5, ZB_ZCL_DRLC_DEVICE_CLASS_MCI_LOADS = 1 << 6, ZB_ZCL_DRLC_DEVICE_CLASS_SIMPLE_LOADS = 1 << 7,
  ZB_ZCL_DRLC_DEVICE_CLASS_EXTERIOR_LIGHTNING = 1 << 8, ZB_ZCL_DRLC_DEVICE_CLASS_INTERIOR_LIGHTNING = 1 << 9, ZB_ZCL_DRLC_DEVICE_CLASS_ELECTRIC_VEHICLE = 1 << 10, ZB_ZCL_DRLC_DEVICE_CLASS_GENERATION_SYSTEMS = 1 << 11
}
 
enum  zb_zcl_drlc_event_status_e {
  ZB_ZCL_DRLC_EVENT_RESERVED_00 = 0x00, ZB_ZCL_DRLC_EVENT_LCE_RECEIVED, ZB_ZCL_DRLC_EVENT_EVENT_STARTED, ZB_ZCL_DRLC_EVENT_EVENT_COMPLETED,
  ZB_ZCL_DRLC_EVENT_OPT_OUT, ZB_ZCL_DRLC_EVENT_OPT_IN, ZB_ZCL_DRLC_EVENT_EVENT_CANCELLED, ZB_ZCL_DRLC_EVENT_EVENT_SUPERSEDED,
  ZB_ZCL_DRLC_EVENT_EVENT_PARTIALLY_OPT_OUT, ZB_ZCL_DRLC_EVENT_EVENT_PARTIALLY_OPT_IN, ZB_ZCL_DRLC_EVENT_EVENT_COMPLETED_NO_USER, ZB_ZCL_DRLC_EVENT_RESERVED_0B,
  ZB_ZCL_DRLC_EVENT_RESERVED_F7 = 0xF7, ZB_ZCL_DRLC_EVENT_REJECTED_INVALID_CANCEL_CMD, ZB_ZCL_DRLC_EVENT_REJECTED_INVALID_EFFECTIVE_TIME, ZB_ZCL_DRLC_EVENT_RESERVED_FA,
  ZB_ZCL_DRLC_EVENT_REJECTED_EXPIRED, ZB_ZCL_DRLC_EVENT_RESERVED_FC, ZB_ZCL_DRLC_EVENT_REJECTED_UNDEFINED_EVENT, ZB_ZCL_DRLC_EVENT_REJECTED,
  ZB_ZCL_DRLC_EVENT_RESERVED_FF
}
 
enum  zb_zcl_drlc_signature_type_e { ZB_ZCL_DRLC_LCE_NO_SIGNATURE = 0x00, ZB_ZCL_DRLC_LCE_SIGNATURE_ECDSA, ZB_ZCL_DRLC_LCE_SIGNATURE_RESERVED }
 

Detailed Description

This section describes DRLC client attributes and common cluster enumerations.

Typedef Documentation

§ zb_zcl_drlc_cli_attr_t

DRLC Client attributes.

See also
SE spec, subclause D.2.3.2

§ zb_zcl_drlc_criticality_levels_t

Criticality Level value applied by the device.

See also
SE spec, Table D-3

§ zb_zcl_drlc_device_class_t

DRLC device classes enumeration.

See also
SE spec, Table D-2.

§ zb_zcl_drlc_event_status_t

DRLC Event Status enum

See also
SE spec, Table D-9

§ zb_zcl_drlc_signature_type_t

DRLC signature type enum

Enumeration Type Documentation

§ zb_zcl_drlc_cli_attr_e

DRLC Client attributes.

See also
SE spec, subclause D.2.3.2
Enumerator
ZB_ZCL_ATTR_DRLC_UTILITY_ENROLLMENT_GROUP 

UtilityEnrollmentGroup attribute. Provides for utilities to assign devices to groups.

ZB_ZCL_ATTR_DRLC_START_RANDOMIZATION_MINUTES 

StartRandomizationMinutes attribute. Represents the maximum number of minutes to be used when randomizing the start of an event.

ZB_ZCL_ATTR_DRLC_DURATION_RANDOMIZATION_MINUTES 

DurationRandomizationMinutes attribute. Represents the maximum number of minutes to be used when randomizing the duration of an event.

ZB_ZCL_ATTR_DRLC_DEVICE_CLASS_VALUE 

DeviceClassValue attribute. Identifies which bits the device will match in the Device Class fields.

§ zb_zcl_drlc_criticality_levels_e

Criticality Level value applied by the device.

See also
SE spec, Table D-3
Enumerator
ZB_ZCL_DRLC_CRITICALITY_LEVEL_0 

Reserved

ZB_ZCL_DRLC_CRITICALITY_LEVEL_1 

Green

ZB_ZCL_DRLC_CRITICALITY_LEVEL_2 

Level 1

ZB_ZCL_DRLC_CRITICALITY_LEVEL_3 

Level 2

ZB_ZCL_DRLC_CRITICALITY_LEVEL_4 

Level 3

ZB_ZCL_DRLC_CRITICALITY_LEVEL_5 

Level 4

ZB_ZCL_DRLC_CRITICALITY_LEVEL_6 

Level 5

ZB_ZCL_DRLC_CRITICALITY_LEVEL_7 

Emergency

ZB_ZCL_DRLC_CRITICALITY_LEVEL_8 

Planned Outage

ZB_ZCL_DRLC_CRITICALITY_LEVEL_9 

Service Disconnect

§ zb_zcl_drlc_device_class_e

DRLC device classes enumeration.

See also
SE spec, Table D-2.
Enumerator
ZB_ZCL_DRLC_DEVICE_CLASS_HVAC 

HVAC Compressor or Furnace

ZB_ZCL_DRLC_DEVICE_CLASS_STRIP_HEATER 

Strip Heaters/Baseboard Heaters

ZB_ZCL_DRLC_DEVICE_CLASS_WATER_HEATER 

Water Heater

ZB_ZCL_DRLC_DEVICE_CLASS_POOL_PUMP 

Pool Pump/Spa/Jacuzzi

ZB_ZCL_DRLC_DEVICE_CLASS_SMART_APPLIANCE 

Smart Appliances

ZB_ZCL_DRLC_DEVICE_CLASS_IRRIGATION_PUMP 

Irrigation Pump

ZB_ZCL_DRLC_DEVICE_CLASS_MCI_LOADS 

Managed Commercial & Industrial (C&I) loads

ZB_ZCL_DRLC_DEVICE_CLASS_SIMPLE_LOADS 

Simple misc. (Residential On/Off) loads

ZB_ZCL_DRLC_DEVICE_CLASS_EXTERIOR_LIGHTNING 

Exterior Lighting

ZB_ZCL_DRLC_DEVICE_CLASS_INTERIOR_LIGHTNING 

Interior Lighting

ZB_ZCL_DRLC_DEVICE_CLASS_ELECTRIC_VEHICLE 

Electric Vehicle

ZB_ZCL_DRLC_DEVICE_CLASS_GENERATION_SYSTEMS 

Generation Systems

§ zb_zcl_drlc_event_status_e

DRLC Event Status enum

See also
SE spec, Table D-9
Enumerator
ZB_ZCL_DRLC_EVENT_RESERVED_00 

Reserved for future use.

ZB_ZCL_DRLC_EVENT_LCE_RECEIVED 

Load Control Event command received

ZB_ZCL_DRLC_EVENT_EVENT_STARTED 

Event started

ZB_ZCL_DRLC_EVENT_EVENT_COMPLETED 

Event completed

ZB_ZCL_DRLC_EVENT_OPT_OUT 

User has chosen to “Opt-Out”, user will not participate in this event

ZB_ZCL_DRLC_EVENT_OPT_IN 

User has chosen to “Opt-In”, user will participate in this event

ZB_ZCL_DRLC_EVENT_EVENT_CANCELLED 

The event has been cancelled

ZB_ZCL_DRLC_EVENT_EVENT_SUPERSEDED 

The event has been superseded

ZB_ZCL_DRLC_EVENT_EVENT_PARTIALLY_OPT_OUT 

Event partially completed with User “Opt-Out”.

ZB_ZCL_DRLC_EVENT_EVENT_PARTIALLY_OPT_IN 

Event partially completed due to User “Opt-In”.

ZB_ZCL_DRLC_EVENT_EVENT_COMPLETED_NO_USER 

Event completed, no User participation (Previous “Opt-Out”).

ZB_ZCL_DRLC_EVENT_RESERVED_0B 

Reserved for future use.

ZB_ZCL_DRLC_EVENT_RESERVED_F7 

Reserved for future use.

ZB_ZCL_DRLC_EVENT_REJECTED_INVALID_CANCEL_CMD 

Rejected - Invalid Cancel Command (Default)

ZB_ZCL_DRLC_EVENT_REJECTED_INVALID_EFFECTIVE_TIME 

Rejected - Invalid Cancel Command (Invalid Effective Time)

ZB_ZCL_DRLC_EVENT_RESERVED_FA 

Reserved

ZB_ZCL_DRLC_EVENT_REJECTED_EXPIRED 

Rejected - Event was received after it had expired
(Current Time > Start Time + Duration)

ZB_ZCL_DRLC_EVENT_RESERVED_FC 

Reserved for future use.

ZB_ZCL_DRLC_EVENT_REJECTED_UNDEFINED_EVENT 

Rejected - Invalid Cancel Command (Undefined Event)

ZB_ZCL_DRLC_EVENT_REJECTED 

Load Control Event command Rejected

ZB_ZCL_DRLC_EVENT_RESERVED_FF 

Reserved for future use.

§ zb_zcl_drlc_signature_type_e

DRLC signature type enum

Enumerator
ZB_ZCL_DRLC_LCE_NO_SIGNATURE 

No Signature

ZB_ZCL_DRLC_LCE_SIGNATURE_ECDSA 

ECDSA

ZB_ZCL_DRLC_LCE_SIGNATURE_RESERVED 

Reserved