Binary Input cluster attribute identifiers.
| Enumerator |
|---|
| ZB_ZCL_ATTR_BINARY_INPUT_ACTIVE_TEXT_ID | This attribute, of type Character string, MAY be used to hold a human readable description of the ACTIVE state of a binary PresentValue.
|
| ZB_ZCL_ATTR_BINARY_INPUT_DESCRIPTION_ID | The Description attribute, of type Character string, MAY be used to hold a description of the usage of the input, output or value, as appropriate to the cluster.
|
| ZB_ZCL_ATTR_BINARY_INPUT_INACTIVE_TEXT_ID | This attribute, of type Character string, MAY be used to hold a human readable description of the INACTIVE state of a binary PresentValue.
|
| ZB_ZCL_ATTR_BINARY_INPUT_OUT_OF_SERVICE_ID | OutOfService attribute.
|
| ZB_ZCL_ATTR_BINARY_INPUT_POLARITY_ID | This attribute, of type enumeration, indicates the relationship between the physical state of the input (or output as appropriate for the cluster) and the logical state represented by a binary PresentValue attribute, when OutOfService is FALSE.
|
| ZB_ZCL_ATTR_BINARY_INPUT_PRESENT_VALUE_ID | PresentValue attribute.
|
| ZB_ZCL_ATTR_BINARY_INPUT_RELIABILITY_ID | The Reliability attribute, of type 8-bit enumeration, provides an indication of whether the PresentValue or the operation of the physical input, output or value in question (as appropriate for the cluster) is reliable as far as can be determined and, if not, why not.
|
| ZB_ZCL_ATTR_BINARY_INPUT_STATUS_FLAG_ID | StatusFlag attribute.
|
| ZB_ZCL_ATTR_BINARY_INPUT_APPLICATION_TYPE_ID | The ApplicationType attribute is an unsigned 32-bit integer that indicates the specific application usage for this cluster.
|