Logo
Developing with ZBOSS for Zigbee
zboss_tcswap.h File Reference

Enumerations

enum  zb_tcswap_dirty_state_t { ZB_TCSWAP_SECUR = 1, ZB_TCSWAP_BINDINGS = 2 }
 

Functions

zb_uint_t zb_tcsw_need_backup (void)
 
zb_bool_t zb_tcsw_is_busy (void)
 
zb_uint_t zb_tcsw_calculate_db_size (void)
 
zb_bool_t zb_tcsw_check_buffer_size (zb_uint_t size)
 
zb_ret_t zb_tcsw_start_backup_db (void)
 
zb_uint_t zb_tcsw_get_portion (zb_uint8_t *buf, zb_uint_t buf_size)
 
zb_ret_t zb_tcsw_start_restore_db (zb_bool_t change_tc_addr)
 
zb_ret_t zc_tcsw_restore_portion (zb_uint8_t *buf, zb_uint_t len)
 
zb_ret_t zc_tcsw_restore_finish (void)
 
void zb_tcsw_enable_passkey_backup (zb_bool_t enable)