#include "zb_address.h"#include "zb_types.h"#include "se/zb_se_device_config.h"#include "zcl/zb_zcl_config.h"#include "zcl/zb_zcl_common.h"#include "zcl/zb_zcl_commands.h"#include "se/zb_se_config.h"#include "zcl/zb_zcl_keep_alive.h"Data Structures | |
| struct | zb_zcl_kec_attrs_s |
| Key Establishment cluster attributes. More... | |
Macros | |
| #define | ZB_ZCL_ATTR_KEY_ESTABLISHMENT_SUITE_ID 0x0000U |
| Key Establishment cluster's attributes IDs. More... | |
| #define | ZB_ZCL_KEY_ESTABLISHMENT_CLUSTER_REVISION_DEFAULT ((zb_uint16_t)0x0002u) |
| Default value for Key Establishment cluster revision global attribute. More... | |
| #define | ZB_KEC_SUPPORTED_CRYPTO_ATTR (KEC_CS1 | KEC_CS2) |
| Attribute value const (supported CryptoSuites) More... | |
| #define | ZB_ZCL_DECLARE_KEC_ATTR_LIST(attr_list, attrs) ZB_ZCL_DECLARE_KEC_ATTRIB_LIST(attr_list, &attrs.kec_suite) |
| Declare attribute list for Key Establishment cluster. More... | |
KeyEstablishmentSuite attribute values | |
| #define | KEC_CS1 (1U << 0) |
| #define | KEC_CS2 (1U << 1) |
Typedefs | |
| typedef zb_uint8_t | zb_kec_key_suite_t |
| Type for KeyEstablishmentSuite attribute values. More... | |
| typedef struct zb_zcl_kec_attrs_s | zb_zcl_kec_attrs_t |
| Key Establishment cluster attributes. More... | |
Functions | |
| zb_ret_t | zb_se_load_ecc_cert (zb_uint16_t suite, zb_uint8_t *ca_public_key, zb_uint8_t *certificate, zb_uint8_t *private_key) |
| Loads device's certificate to NVRAM. More... | |
| zb_ret_t | zb_se_erase_ecc_cert (zb_uint8_t suite_no, zb_uint8_t *issuer, zb_uint8_t *subject) |
| Erases device's certificate from NVRAM. More... | |
| zb_bool_t | zb_se_has_valid_key (zb_uint16_t addr) |
| Checks availability of valid keypair for the specified remote device using its short address. More... | |
| zb_bool_t | zb_se_has_valid_key_by_ieee (zb_ieee_addr_t addr) |
| Checks availability of valid keypair for the specified remote device using its address as a keypair established between a pair of devices. More... | |
| zb_ret_t | zb_se_debug_get_link_key (zb_uint16_t addr, zb_uint8_t link_key[ZB_CCM_KEY_SIZE]) |
| Retrieves APS link key or TCLK for the remote device. More... | |
| zb_ret_t | zb_se_debug_get_link_key_by_long (zb_ieee_addr_t ieee, zb_uint8_t link_key[ZB_CCM_KEY_SIZE]) |
| Retrieves APS link key or TCLK for the remote device using it's long address. More... | |
| zb_ret_t | zb_se_debug_get_nwk_key (zb_uint8_t key[ZB_CCM_KEY_SIZE]) |
| Retrieves current NWK key. More... | |
| zb_ret_t | zb_se_debug_get_ic_key (zb_uint8_t key[ZB_CCM_KEY_SIZE]) |
| Retrieves APS link key generated from the current installcode. More... | |
| void | zb_se_start_aps_key_establishment (zb_uint8_t param, zb_uint16_t addr) |
| Starts procedure of partner APS link key establishment with the specified device. More... | |
| zb_ret_t | zb_se_service_discovery_start (zb_uint8_t endpoint) |
| Puts device into the Service Discovery state. More... | |
| void | zb_se_service_discovery_stop () |
| Stops Service Discovery process started with zb_se_service_discovery_start(). More... | |
| void | zb_se_service_discovery_set_multiple_commodity_enabled (zb_uint8_t enabled) |
| Allows enabling or disabling support for multiple commodity networks. More... | |
| void | zb_se_service_discovery_bind_req (zb_uint8_t param, zb_ieee_addr_t dst_ieee, zb_uint16_t dst_ep) |
| Sends Bind Request command to the discovered SE device. More... | |