Logo
Developing with ZBOSS for Zigbee
zb_zcl_addr_s::zb_zcl_addr_u Union Reference

#include <zb_zcl_common.h>

Data Fields

zb_uint16_t short_addr
 
zb_uint32_t src_id
 
zb_ieee_addr_t ieee_addr
 

Field Documentation

§ ieee_addr

zb_ieee_addr_t zb_zcl_addr_s::zb_zcl_addr_u::ieee_addr

Full IEEE-address of ZGPD

§ short_addr

zb_uint16_t zb_zcl_addr_s::zb_zcl_addr_u::short_addr

Zigbee short address

§ src_id

zb_uint32_t zb_zcl_addr_s::zb_zcl_addr_u::src_id

Source ID of ZGPD


The documentation for this union was generated from the following file: