Logo
Developing with ZBOSS for Zigbee
zgp_tbl_ent_s Struct Reference

#include <zboss_api_zgp.h>

Data Fields

zb_zgpd_addr_t zgpd_id
 
zb_uint16_t options
 
zb_uint16_t zgpd_assigned_alias
 
zb_uint32_t security_counter
 
zb_uint8_t zgpd_key [16U]
 
zb_uint8_t endpoint
 
zb_uint8_t sec_options
 
zb_uint8_t groupcast_radius
 
zb_uint8_t is_sink
 
union {
   struct zgp_proxy_tbl_ent_s {
      zb_uint16_t   ext_options
 
      struct zgp_lwsink_addr_list_s {
         zb_address_ieee_ref_t   addr_ref
 
      }   lwsaddr [2U]
 
      zgp_pair_group_list_t   sgrp [2U]
 
   }   proxy
 
   struct zgp_sink_tbl_ent_s {
      zb_uint8_t   device_id
 
      zgp_pair_group_list_t   sgrp [2U]
 
      zb_uint8_t   match_dev_tbl_idx
 
      zb_ieee_addr_t   ieee_addr
 
   }   sink
 
u
 

Field Documentation

§ addr_ref

zb_address_ieee_ref_t zgp_tbl_ent_s::addr_ref

§ device_id

zb_uint8_t zgp_tbl_ent_s::device_id

ZGPD Device ID from Commissioning frame

See also
zb_zgpd_dev_id_t

§ endpoint

zb_uint8_t zgp_tbl_ent_s::endpoint

Endpoint pair of IEEE:EP if App ID is 010.

§ ext_options

zb_uint16_t zgp_tbl_ent_s::ext_options

§ groupcast_radius

zb_uint8_t zgp_tbl_ent_s::groupcast_radius

To limit the range of the groupcast

§ ieee_addr

zb_ieee_addr_t zgp_tbl_ent_s::ieee_addr

Extension to the table (field is not presented in specification).

Dest IEEE address to use in GPT to GPD packets even if GPD is identified by SrcID

§ is_sink

zb_uint8_t zgp_tbl_ent_s::is_sink

§ lwsaddr

struct { ... } ::zgp_proxy_tbl_ent_s::zgp_lwsink_addr_list_s zgp_tbl_ent_s::lwsaddr[ 2U ]

§ match_dev_tbl_idx

zb_uint8_t zgp_tbl_ent_s::match_dev_tbl_idx

index in matching table matched by device_id or app_info.manuf_model_id

§ options

zb_uint16_t zgp_tbl_ent_s::options

The options for the reception from ZGPD

§ proxy

struct { ... } ::zgp_proxy_tbl_ent_s zgp_tbl_ent_s::proxy

§ sec_options

zb_uint8_t zgp_tbl_ent_s::sec_options

Security options

§ security_counter

zb_uint32_t zgp_tbl_ent_s::security_counter

The incoming security frame counter for ZGPD

§ sgrp

zgp_pair_group_list_t zgp_tbl_ent_s::sgrp[2U]

§ sink

struct { ... } ::zgp_sink_tbl_ent_s zgp_tbl_ent_s::sink

§ u

union { ... } zgp_tbl_ent_s::u

§ zgpd_assigned_alias

zb_uint16_t zgp_tbl_ent_s::zgpd_assigned_alias

The commissioned 16-bit ID to be used as alias for ZGPD

§ zgpd_id

zb_zgpd_addr_t zgp_tbl_ent_s::zgpd_id

ID of the paired ZGPD

§ zgpd_key

zb_uint8_t zgp_tbl_ent_s::zgpd_key[16U]

Security key for the GPD


The documentation for this struct was generated from the following file: