Logo
Developing with ZBOSS for Zigbee
zgp_runtime_app_tbl_ent_s Struct Reference

#include <zboss_api_zgp.h>

Data Fields

zb_uint8_t status
 
zb_uint8_t receive_reports [(((3U)+7U)/8U)]
 
zb_uint8_t reply_buf
 
zb_bool_t need_reply
 
zgp_app_tbl_ent_t base
 

Field Documentation

§ base

zgp_app_tbl_ent_t zgp_runtime_app_tbl_ent_s::base

§ need_reply

zb_bool_t zgp_runtime_app_tbl_ent_s::need_reply

§ receive_reports

zb_uint8_t zgp_runtime_app_tbl_ent_s::receive_reports[((( 3U)+7U)/8U)]

§ reply_buf

zb_uint8_t zgp_runtime_app_tbl_ent_s::reply_buf

§ status

zb_uint8_t zgp_runtime_app_tbl_ent_s::status

The documentation for this struct was generated from the following file: