Raw report descriptor received from the GPD. More...
#include <zboss_api_zgp.h>
Data Fields | |
| zb_uint8_t | len |
| zb_uint8_t | data [32U] |
Raw report descriptor received from the GPD.
| zb_uint8_t zgp_raw_report_desc_s::data[32U] |
array of not parsed zgp_data_point_desc_t
| zb_uint8_t zgp_raw_report_desc_s::len |
total len, in octets, of the current report descriptor.