Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_scan_res_s Struct Reference

Parsed Commissioning.ScanResponse structure. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 Inter-PAN transaction identifier. More...
 
zb_uint8_t rssi_correction
 RSSI correction. More...
 
zb_uint8_t zb_info
 Zigbee device information. More...
 
zb_uint8_t zll_info
 Touchlink information. More...
 
zb_uint16_t key_bitmask
 Key bitmask. More...
 
zb_uint32_t resp_id
 Response identifier. More...
 
zb_ext_pan_id_t ext_pan_id
 Extended Pan ID. More...
 
zb_uint8_t nwk_upd_id
 Network update identifier. More...
 
zb_uint8_t channel
 Logical channel. More...
 
zb_uint16_t pan_id
 Pan ID. More...
 
zb_uint16_t nwk_addr
 Network address. More...
 
zb_uint8_t n_subdevs
 Number of sub-devices. More...
 
zb_uint8_t group_ids_total
 Total group identifiers. More...
 
zb_zll_commissioning_ep_info_t endpoint_info
 Endpoint information. Shall be present if device has only single endpoint. More...
 

Detailed Description

Parsed Commissioning.ScanResponse structure.

See also
ZCL spec, subclause 13.3.2.2.1.

Field Documentation

§ channel

zb_uint8_t zb_zll_commissioning_scan_res_s::channel

Logical channel.

§ endpoint_info

zb_zll_commissioning_ep_info_t zb_zll_commissioning_scan_res_s::endpoint_info

Endpoint information. Shall be present if device has only single endpoint.

§ ext_pan_id

zb_ext_pan_id_t zb_zll_commissioning_scan_res_s::ext_pan_id

Extended Pan ID.

§ group_ids_total

zb_uint8_t zb_zll_commissioning_scan_res_s::group_ids_total

Total group identifiers.

§ key_bitmask

zb_uint16_t zb_zll_commissioning_scan_res_s::key_bitmask

Key bitmask.

§ n_subdevs

zb_uint8_t zb_zll_commissioning_scan_res_s::n_subdevs

Number of sub-devices.

§ nwk_addr

zb_uint16_t zb_zll_commissioning_scan_res_s::nwk_addr

Network address.

§ nwk_upd_id

zb_uint8_t zb_zll_commissioning_scan_res_s::nwk_upd_id

Network update identifier.

§ pan_id

zb_uint16_t zb_zll_commissioning_scan_res_s::pan_id

Pan ID.

§ resp_id

zb_uint32_t zb_zll_commissioning_scan_res_s::resp_id

Response identifier.

§ rssi_correction

zb_uint8_t zb_zll_commissioning_scan_res_s::rssi_correction

RSSI correction.

§ trans_id

zb_uint32_t zb_zll_commissioning_scan_res_s::trans_id

Inter-PAN transaction identifier.

§ zb_info

zb_uint8_t zb_zll_commissioning_scan_res_s::zb_info

Zigbee device information.

§ zll_info

zb_uint8_t zb_zll_commissioning_scan_res_s::zll_info

Touchlink information.


The documentation for this struct was generated from the following file: