Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. More...
#include <zboss_api_zgp.h>
Data Fields | |
| zb_uint8_t | contact_status |
| zb_uint8_t | contact_bitmask |
Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry.
| zb_uint8_t zb_zgps_mapping_entry_generic_switch_option_data_s::contact_bitmask |
| zb_uint8_t zb_zgps_mapping_entry_generic_switch_option_data_s::contact_status |