MAC-Split device boot parameters. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint32_t | dev_version |
| zb_ieee_addr_t | extended_address |
MAC-Split device boot parameters.
MAC-Split passes this parameter to application when device is booted.
| zb_uint32_t zb_zdo_signal_macsplit_dev_boot_params_s::dev_version |
MAC-Split device version
| zb_ieee_addr_t zb_zdo_signal_macsplit_dev_boot_params_s::extended_address |
The 64-bit (IEEE) address assigned to the device.