Logo
Developing with ZBOSS for Zigbee
zb_zdo_secur_get_auth_level_rsp_s Struct Reference

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t tsn
 
zb_uint8_t status
 
zb_ieee_addr_t target_ieee
 
zb_initial_join_auth_t initial_join_auth
 
zb_post_join_key_upd_method_t key_upd_method
 

Field Documentation

§ initial_join_auth

zb_initial_join_auth_t zb_zdo_secur_get_auth_level_rsp_s::initial_join_auth

§ key_upd_method

zb_post_join_key_upd_method_t zb_zdo_secur_get_auth_level_rsp_s::key_upd_method

§ status

zb_uint8_t zb_zdo_secur_get_auth_level_rsp_s::status

§ target_ieee

zb_ieee_addr_t zb_zdo_secur_get_auth_level_rsp_s::target_ieee

§ tsn

zb_uint8_t zb_zdo_secur_get_auth_level_rsp_s::tsn

The documentation for this struct was generated from the following file: