Next PAN ID change parameters Stack sends set_configuration_req to the device with set values. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | dst_addr |
| zb_uint16_t | next_panid_change |
Next PAN ID change parameters Stack sends set_configuration_req to the device with set values.
| zb_uint16_t zb_zdo_next_panid_change_parameters_s::dst_addr |
destination address
| zb_uint16_t zb_zdo_next_panid_change_parameters_s::next_panid_change |
nwkNextPanId, this field indicates the next PAN ID that will be used once a Network Update command is received to change PAN IDs. A value 0xFFFF allows any PAN ID to be accepted