NeighborTableList Record Format for Mgmt_Lqi_resp. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_ext_pan_id_t | ext_pan_id |
| zb_ieee_addr_t | ext_addr |
| zb_uint16_t | network_addr |
| zb_uint8_t | type_flags |
| zb_uint8_t | permit_join |
| zb_uint8_t | depth |
| zb_uint8_t | lqa |
NeighborTableList Record Format for Mgmt_Lqi_resp.
| zb_uint8_t zb_zdo_neighbor_table_record_s::depth |
The tree depth of the neighbor device.
| zb_ieee_addr_t zb_zdo_neighbor_table_record_s::ext_addr |
64-bit IEEE address that is unique to every device.
| zb_ext_pan_id_t zb_zdo_neighbor_table_record_s::ext_pan_id |
64-bit extended Pan ID of the neighboring device.
| zb_uint8_t zb_zdo_neighbor_table_record_s::lqa |
The estimated link quality for RF transmissions from this device
| zb_uint16_t zb_zdo_neighbor_table_record_s::network_addr |
The 16-bit network address of the neighboring device
| zb_uint8_t zb_zdo_neighbor_table_record_s::permit_join |
An indication of whether the neighbor device is accepting join requests
| zb_uint8_t zb_zdo_neighbor_table_record_s::type_flags |
device type, rx_on_when_idle, relationship