Logo
Developing with ZBOSS for Zigbee
zb_zdo_mgmt_beacon_survey_param_s Struct Reference

Parameters for beacon_survey_req command. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t channel_page_cnt
 
zb_uint32_t channel_page_list [10U]
 
zb_uint8_t config_mask
 
zb_uint16_t dst_addr
 

Detailed Description

Parameters for beacon_survey_req command.

Field Documentation

§ channel_page_cnt

zb_uint8_t zb_zdo_mgmt_beacon_survey_param_s::channel_page_cnt

§ channel_page_list

zb_uint32_t zb_zdo_mgmt_beacon_survey_param_s::channel_page_list[10U]

§ config_mask

zb_uint8_t zb_zdo_mgmt_beacon_survey_param_s::config_mask

§ dst_addr

zb_uint16_t zb_zdo_mgmt_beacon_survey_param_s::dst_addr

destination address


The documentation for this struct was generated from the following file: