Logo
Developing with ZBOSS for Zigbee
zb_zdo_get_diag_data_resp_params_s Struct Reference

#include <zboss_api_zdo.h>

Data Fields

zb_ret_t status
 
zb_uint16_t short_address
 
zb_uint8_t lqi
 
zb_int8_t rssi
 

Field Documentation

§ lqi

zb_uint8_t zb_zdo_get_diag_data_resp_params_s::lqi

§ rssi

zb_int8_t zb_zdo_get_diag_data_resp_params_s::rssi

§ short_address

zb_uint16_t zb_zdo_get_diag_data_resp_params_s::short_address

§ status

zb_ret_t zb_zdo_get_diag_data_resp_params_s::status

The documentation for this struct was generated from the following file: