Logo
Developing with ZBOSS for Zigbee
zb_zdo_ed_scan_param_s Struct Reference

#include <zboss_api_zdo.h>

Data Fields

zb_callback_t cb
 
zb_nlme_ed_scan_request_t nwk_param
 

Detailed Description

Parameters for zb_zdo_ed_scan_request call.

Field Documentation

§ cb

zb_callback_t zb_zdo_ed_scan_param_s::cb

Callback that will be called after ED scan finished.

§ nwk_param

zb_nlme_ed_scan_request_t zb_zdo_ed_scan_param_s::nwk_param

Parameters with which scan will be performed: Channels and scan duration.


The documentation for this struct was generated from the following file: