Developing with ZBOSS for Zigbee
Data Fields
zb_zcl_tunnel_io_slot_s Struct Reference
Zigbee stack API
»
ZCL API
»
ZCL clusters
»
ZCL Tunnel cluster
#include <zb_zcl_tunnel.h>
Data Fields
zb_zcl_tunnel_io_param_t
io_param
zb_uint16_t
offset
zb_uint8_t
seq
Field Documentation
§
io_param
zb_zcl_tunnel_io_param_t
zb_zcl_tunnel_io_slot_s::io_param
§
offset
zb_uint16_t
zb_zcl_tunnel_io_slot_s::offset
§
seq
zb_uint8_t
zb_zcl_tunnel_io_slot_s::seq
The documentation for this struct was generated from the following file:
/conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/
zb_zcl_tunnel.h
Copyright (c) 2012-2022 DSR Corporation, Golden CO, USA.
http://www.dsr-zboss.com
http://www.dsr-corporation.com
ZBOSS documentation. Wed Oct 29 2025.