#include <zb_zcl_prepayment.h>
Debt/Credit Status Command Payload
| zb_int32_t zb_zcl_prepayment_snapshot_payload_s::accumulated_debt |
The AccumulatedDebt field represents the total amount of debt remaining on the Metering Device, measured in a base unit of Currency with the decimal point located as indicated by the Trailing Digits field, as defined in the Price cluster.
| zb_int32_t zb_zcl_prepayment_snapshot_payload_s::credit_remaining |
The CreditRemaining field represents the amount of credit remaining on the Metering Device. If Monetary based, this field is measured in a base unit of Currency or in Units, with the decimal point.
| struct { ... } zb_zcl_prepayment_snapshot_payload_s::debt_credit_status |
| zb_int32_t zb_zcl_prepayment_snapshot_payload_s::emergency_credit_remaining |
The EmergencyCreditRemaining field represents the amount of Emergency Credit still available on the Metering Device. If Monetary based, this field is measured in a base unit of Currency or in Units, with the decimal point
| zb_uint8_t zb_zcl_prepayment_snapshot_payload_s::snapshot_payload_type |
| zb_uint32_t zb_zcl_prepayment_snapshot_payload_s::type_1_debt_remaining |
The Type1DebtRemaining field represents the amount of Type 1 debt remaining on the Metering Device, measured in base unit of Currency with the decimal point located as indicated by the Trailing Digits field, as defined in the Price cluster.
| zb_uint32_t zb_zcl_prepayment_snapshot_payload_s::type_2_debt_remaining |
The Type2DebtRemaining field represents the amount of Type 2 debt remaining on the Metering Device, measured in base unit of Currency with the decimal point located as indicated by the TrailingDigits field, as defined in the Price cluster.
| zb_uint32_t zb_zcl_prepayment_snapshot_payload_s::type_3_debt_remaining |
The Type3DebtRemaining field represents the amount of Type 3 debt remaining on the Metering Device, measured in base unit of Currency with the decimal point located as indicated by the TrailingDigits field, as defined in the Price cluster.
| union { ... } zb_zcl_prepayment_snapshot_payload_s::u |