Logo
Developing with ZBOSS for Zigbee
zb_zcl_ota_upgrade_data_s Struct Reference

Structure representation of OTA file on server side. More...

#include <zb_zcl_ota_upgrade.h>

Data Fields

zb_zcl_ota_upgrade_file_header_tfile_header
 
zb_uint32_t upgrade_time
 

Detailed Description

Structure representation of OTA file on server side.

Field Documentation

§ file_header

zb_zcl_ota_upgrade_file_header_t* zb_zcl_ota_upgrade_data_s::file_header

§ upgrade_time

zb_uint32_t zb_zcl_ota_upgrade_data_s::upgrade_time

The documentation for this struct was generated from the following file: