Structure representation of Event Notification command.
More...
#include <zb_zcl_en50523_appliance_events_and_alerts.h>
Structure representation of Event Notification command.
- Parameters
-
| event_header | - Event header field |
| event_identification | - Event Identification field, see zb_zcl_en50523_appl_ev_and_alerts_event_identification_e |
§ event_header
| zb_uint8_t zb_zcl_en50523_appl_ev_and_alerts_event_notif_s::event_header |
§ event_identification
| zb_uint8_t zb_zcl_en50523_appl_ev_and_alerts_event_notif_s::event_identification |
The documentation for this struct was generated from the following file: