Logo
Developing with ZBOSS for Zigbee
zb_zcl_direct_configuration_configure_interface_resp_s Struct Reference

Configure Interface Response parameters. More...

#include <zb_zcl_direct_configuration.h>

Data Fields

zb_uint8_t status
 
zb_uint8_t interface_state
 

Detailed Description

Configure Interface Response parameters.

Field Documentation

§ interface_state

zb_uint8_t zb_zcl_direct_configuration_configure_interface_resp_s::interface_state

Current Interface State,

See also
zb_zcl_direct_configuration_interface_state

§ status

zb_uint8_t zb_zcl_direct_configuration_configure_interface_resp_s::status

Command processing status


The documentation for this struct was generated from the following file: