#include <zb_zcl_calendar.h>
Special Day Entry A SpecialDayEntry consists of the Special Day Date and a reference (Day ID Ref) to the related Day Profile entry. The dates of the Special Day Table must be arranged in ascending order.
- See also
- SE spec, Figure D-147 - SpecialDayEntry Sub-Payload
-
zb_zcl_calendar_publish_special_days_payload_t::special_day_entry
§ day_id_ref
| zb_uint8_t zb_zcl_calendar_special_day_entry_s::day_id_ref |
§ special_day_date
| zb_uint32_t zb_zcl_calendar_special_day_entry_s::special_day_date |
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_calendar.h