#include <zb_zcl_calendar.h>
PublishWeekProfile command payload
- See also
- SE spec, subclause D.9.2.3.3.2 and Figure D-143 - PublishWeekProfile Command Payload
§ day_id_ref_friday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_friday |
§ day_id_ref_monday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_monday |
Day ID Ref Monday until Day ID Ref Sunday (mandatory): Reference to the related Day Profile entry.
§ day_id_ref_saturday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_saturday |
§ day_id_ref_sunday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_sunday |
§ day_id_ref_thursday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_thursday |
§ day_id_ref_tuesday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_tuesday |
§ day_id_ref_wednesday
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::day_id_ref_wednesday |
§ issuer_calendar_id
| zb_uint32_t zb_zcl_calendar_publish_week_profile_payload_s::issuer_calendar_id |
Unique identifier generated by the commodity supplier. All parts of a calendar instance shall have the same Issuer Calendar ID.
§ issuer_event_id
| zb_uint32_t zb_zcl_calendar_publish_week_profile_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
§ provider_id
| zb_uint32_t zb_zcl_calendar_publish_week_profile_payload_s::provider_id |
An unsigned 32-bit field containing a unique identifier for the commodity provider.
§ week_id
| zb_uint8_t zb_zcl_calendar_publish_week_profile_payload_s::week_id |
Unique identifier generated by the commodity supplier. The Week ID is used as reference to assign a Week Profile to a Season Entry. When generating calendars, Week IDs shall be allocated sequentially, starting from 1.
The documentation for this struct was generated from the following file:
- /conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_calendar.h