Logo
Developing with ZBOSS for Zigbee
zb_bdb_signal_touchlink_nwk_started_params_s Struct Reference

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t device_ieee_addr
 
zb_uint8_t endpoint
 
zb_uint16_t profile_id
 

Field Documentation

§ device_ieee_addr

zb_ieee_addr_t zb_bdb_signal_touchlink_nwk_started_params_s::device_ieee_addr

address of device that started the network

§ endpoint

zb_uint8_t zb_bdb_signal_touchlink_nwk_started_params_s::endpoint

§ profile_id

zb_uint16_t zb_bdb_signal_touchlink_nwk_started_params_s::profile_id

The documentation for this struct was generated from the following file: