Data Structures | |
| struct | zgp_to_zb_cmd_mapping_s |
| Mapping of ZGPD command ID to Zigbee ZCL command ID. More... | |
| struct | zb_zgps_mapping_entry_additional_info_option_selector_s |
| Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_generic_switch_option_data_s |
| Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_generic_switch_option_s |
| Mapping table entry additional info generic switch option structure. More... | |
| struct | zb_zgps_mapping_entry_additional_info_option_record_s |
| Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_additional_info_s |
| Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry. More... | |
| struct | zb_zgps_mapping_entry_s |
| Mapping table entry structure. More... | |
Macros | |
| #define | ZB_ZGP_ZCL_CMD_ID_UNDEFINED (0xff) |
| #define | ZB_ZGP_ZCL_CLUSTER_ID_UNDEFINED (0xffff) |
| #define | ZB_GPDF_CMD_UNDEFINED (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_PASS_RAW_GPDF_TO_APP (0xfc) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_NO_PAIRS (0xfd) |
| #define | ZB_ZGP_MAPPING_ENTRY_ENDPOINT_ALL_ARE_MATCHED (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_NO_PAYLOAD (0x00) |
| #define | ZB_ZGP_MAPPING_ENTRY_GPDF_PAYLOAD (0xff) |
| #define | ZB_ZGP_MAPPING_ENTRY_PARSED_PAYLOAD (0xfe) |
| #define | ZB_ZGP_MAPPING_ENTRY_OPTIONS(app_id, add_info_present) (((((add_info_present) & 0x01) << 3)) | ((app_id) & 0x07)) |
| #define | ZB_ZGP_MAPPING_ENTRY_OPTIONS_IS_ADDITIONAL_INFO_PRESENT(options) (((options) >> 3) & 0x01) |
| #define | ZB_ZGP_GET_MAPPING_ENTRY_ZCL_PAYLOAD_PTR(entry) (&entry->zcl_payload_length+sizeof(entry->zcl_payload_length)) |
| #define | ZB_ZGP_SET_MAPPING_TABLE(table_ptr, table_size_ptr) |
| Set mapping table information that is used to fill ZGP command - ZCL cluster mapping table. More... | |
| #define | ZB_ZGP_REGISTER_COMM_REQ_CB(cb) |
| Register commissioning request callback. More... | |
| #define | ZB_ZGP_REGISTER_APP_CIC_CB(cb) |
| Register application commissioning indication callback. More... | |
| #define | ZB_ZGP_FILL_GPS_SECURITY_LEVEL(sec_lvl, with_link_key, involve_tc) (((sec_lvl) & 3U) | ((!!(with_link_key)) << 2U) | ((!!(involve_tc)) << 3U)) |
Typedefs | |
| typedef struct zgp_to_zb_cmd_mapping_s | zgp_to_zb_cmd_mapping_t |
| Mapping of ZGPD command ID to Zigbee ZCL command ID. More... | |
| typedef struct zb_zgps_mapping_entry_additional_info_option_selector_s | zb_zgps_mapping_entry_additional_info_option_selector_t |
| Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry. More... | |
| typedef struct zb_zgps_mapping_entry_generic_switch_option_data_s | zb_zgps_mapping_entry_generic_switch_option_data_t |
| Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry. More... | |
| typedef struct zb_zgps_mapping_entry_generic_switch_option_s | zb_zgps_mapping_entry_generic_switch_option_t |
| Mapping table entry additional info generic switch option structure. More... | |
| typedef struct zb_zgps_mapping_entry_additional_info_option_record_s | zb_zgps_mapping_entry_additional_info_option_record_t |
| Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry. More... | |
| typedef struct zb_zgps_mapping_entry_additional_info_s | zb_zgps_mapping_entry_additional_info_t |
| Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry. More... | |
| typedef struct zb_zgps_mapping_entry_s | zb_zgps_mapping_entry_t |
| Mapping table entry structure. More... | |
| typedef void(* | zb_zgp_app_comm_ind_cb_t) (zb_zgpd_id_t *zgpd_id, zb_uint8_t param) |
| Application callback, indication of the attempted commissioning in GPS operational mode. More... | |
Enumerations | |
| enum | zb_zgps_mapping_entry_8bit_vector_option_ids_e { ZB_ZGPS_MAPPING_ENTRY_8BIT_VECTOR_OPTION_ID_GENERIC_SWITCH_COMMAND_EXECUTION = 0U } |
| A.3.6.2.2.1.1 OptionIDs for GPD 8-bit vector commands. More... | |
| enum | zb_zgps_mapping_entry_compact_attr_report_option_ids_e { ZB_ZGPS_MAPPING_ENTRY_COMPACT_ATTR_REPORT_REPORTABLE = 0U } |
| A.3.6.2.2.1.2 OptionIDs for GPD Compact Attribute Reporting. More... | |
Functions | |
| void | zb_zgps_start_commissioning (zb_time_t timeout) |
| Puts ZGPS into the commissioning mode. More... | |
| void | zb_zgps_start_commissioning_on_ep (zb_uint8_t ep, zb_time_t timeout) |
| Puts ZGPS into the commissioning mode on a specific endpoint. More... | |
| void | zb_zgps_stop_commissioning (void) |
| Switches ZGPS back to the operational mode from the commissioning mode. More... | |
| void | zb_zgps_accept_commissioning (zb_bool_t accept) |
| Accepts/rejects ZGPD commissioning attempt. More... | |
| void | zb_zgps_delete_zgpd (zb_uint8_t buf_ref, zb_zgpd_id_t *zgpd_id) |
| Removes all information about ZGPD from the stack. More... | |
| void | zb_zgps_delete_all_zgpd (void) |
| Removes all information about all ZGPDs from the stack. More... | |
| void | zb_zgps_get_diag_data (zb_zgpd_id_t *zgpd_id, zb_uint8_t *lqi, zb_int8_t *rssi) |
| Retrieves LQI and RSSI last received from the ZGPD. More... | |
| void | zb_zgps_set_security_level (zb_uint_t level) |
| Sets gpsSecurityLevel GP cluster attribute of GPCB. More... | |
| zb_uint8_t | zb_zgps_get_security_level (void) |
| Gets gpsSecurityLevel GP cluster attribute of the GPCB. More... | |
| void | zb_zgp_set_shared_security_key_type (zb_uint_t key_type) |
| Sets gpSharedSecurityKeyType GP cluster attribute. More... | |
| void | zb_zgp_set_shared_security_key (zb_uint8_t *key) |
| Sets gpSharedSecurityKey GP cluster attribute. More... | |
| void | zb_zgps_set_commissioning_exit_mode (zb_uint_t cem) |
| Sets gpsCommissioningExitMode GP cluster attribute. More... | |
| void | zb_zgps_set_communication_mode (zgp_communication_mode_t mode) |
| Sets gpsCommunicationMode GP cluster attribute of the GPCB. More... | |
| zb_ret_t | zb_zgp_convert_8bit_vector (zb_uint8_t vector_8bit_cmd_id, zb_uint8_t switch_type, zb_uint8_t num_of_contacts, zb_uint8_t contact_status, zb_uint8_t *zgp_cmd_out) |
| The function may be overridden by the application to implement custom translation of 8-bit vector command (generic switch). More... | |
| void | zb_zgp_gpdf_raw_indication (zb_bufid_t buf_ref) |
| Frees the incoming raw GPDF packet (buffer). This function can be overridden by the application to implement custom handling of the buffer. More... | |
| void | zb_zgp_set_skip_gpdf (zb_uint8_t skip) |
| Sets ZBOSS to skip all incoming GPDFs. More... | |
| zb_uint8_t | zb_zgp_get_skip_gpdf (void) |
| Checks if ZBOSS skips all incoming GPDFs. More... | |
| void | zb_zgp_sync_pib (zb_uint8_t param) |
| Calls MLME-SET.request to sync SKIP_ALL_GPF attribute. More... | |
| #define ZB_GPDF_CMD_UNDEFINED (0xff) |
| #define ZB_ZGP_FILL_GPS_SECURITY_LEVEL | ( | sec_lvl, | |
| with_link_key, | |||
| involve_tc | |||
| ) | (((sec_lvl) & 3U) | ((!!(with_link_key)) << 2U) | ((!!(involve_tc)) << 3U)) |
Fill security level constant to be passed to zb_zgps_set_security_level()
Described in A.3.3.2.6 gpsSecurityLevel attribute.
| sec_lvl | zb_zgp_security_level_e Minimal GPD Security Level sub-field contains the minimum gpdSecurityLevel this sink accepts |
| with_link_key | 1 bit - Protection with the gpLinkKey sub-field, indicates if the GPDs attempting the pairing are required to support protecting the over-the-air exchange of the GPD Key |
| involve_tc | always zero for the current GPPB specification |
| #define ZB_ZGP_GET_MAPPING_ENTRY_ZCL_PAYLOAD_PTR | ( | entry | ) | (&entry->zcl_payload_length+sizeof(entry->zcl_payload_length)) |
| #define ZB_ZGP_MAPPING_ENTRY_ENDPOINT_ALL_ARE_MATCHED (0xff) |
| #define ZB_ZGP_MAPPING_ENTRY_ENDPOINT_NO_PAIRS (0xfd) |
| #define ZB_ZGP_MAPPING_ENTRY_ENDPOINT_PASS_RAW_GPDF_TO_APP (0xfc) |
| #define ZB_ZGP_MAPPING_ENTRY_GPDF_PAYLOAD (0xff) |
| #define ZB_ZGP_MAPPING_ENTRY_NO_PAYLOAD (0x00) |
| #define ZB_ZGP_MAPPING_ENTRY_OPTIONS | ( | app_id, | |
| add_info_present | |||
| ) | (((((add_info_present) & 0x01) << 3)) | ((app_id) & 0x07)) |
| #define ZB_ZGP_MAPPING_ENTRY_OPTIONS_IS_ADDITIONAL_INFO_PRESENT | ( | options | ) | (((options) >> 3) & 0x01) |
| #define ZB_ZGP_MAPPING_ENTRY_PARSED_PAYLOAD (0xfe) |
| #define ZB_ZGP_REGISTER_APP_CIC_CB | ( | cb | ) |
Register application commissioning indication callback.
| cb | [in] Application commissioning indication callback (zb_zgp_app_comm_ind_cb_t) |
| #define ZB_ZGP_REGISTER_COMM_REQ_CB | ( | cb | ) |
Register commissioning request callback.
| cb | [in] Commissioning request callback (zb_zgp_comm_req_cb_t) |
| #define ZB_ZGP_SET_MAPPING_TABLE | ( | table_ptr, | |
| table_size_ptr | |||
| ) |
Set mapping table information that is used to fill ZGP command - ZCL cluster mapping table.
| [in] | table_ptr | Mapping information, pointer to array of type zb_zgps_mapping_entry_t |
| [in] | table_size_ptr | pointer to size of the table - max entry number what can be iterated |
| #define ZB_ZGP_ZCL_CLUSTER_ID_UNDEFINED (0xffff) |
| #define ZB_ZGP_ZCL_CMD_ID_UNDEFINED (0xff) |
| typedef void( * zb_zgp_app_comm_ind_cb_t) (zb_zgpd_id_t *zgpd_id, zb_uint8_t param) |
Application callback, indication of the attempted commissioning in GPS operational mode.
Application commissioning indication callback notifies application about commissioning attempt from ZGPD. Callback is called when commissioning frame or notification is received from ZGPD. Callback provides to zgpd_id and full incoming packet's data. Based on these parameters user application should decide further actions.
Application commissioning indication callback should be set during ZGP initialization using ZB_ZGP_REGISTER_APP_CIC_CB macro.
| [in] | zgpd_id | ZGPD ID |
| [in] | param | buffer index, containing GPDF |
| typedef struct zb_zgps_mapping_entry_additional_info_option_record_s zb_zgps_mapping_entry_additional_info_option_record_t |
Mapping table entry additional info option record structure A.3.6.2.2 GPD application functionality translation Figure 83 – Format of the Option record field of the Translation Table entry.
| typedef struct zb_zgps_mapping_entry_additional_info_option_selector_s zb_zgps_mapping_entry_additional_info_option_selector_t |
Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry.
Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry.
| typedef struct zb_zgps_mapping_entry_generic_switch_option_data_s zb_zgps_mapping_entry_generic_switch_option_data_t |
Mapping table entry additional info generic switch option data structure Figure 85 – Format of the Option data of the Generic switch command execution option of the Translation Table entry.
| typedef struct zb_zgps_mapping_entry_generic_switch_option_s zb_zgps_mapping_entry_generic_switch_option_t |
Mapping table entry additional info generic switch option structure.
| typedef struct zb_zgps_mapping_entry_s zb_zgps_mapping_entry_t |
Mapping table entry structure.
| typedef struct zgp_to_zb_cmd_mapping_s zgp_to_zb_cmd_mapping_t |
Mapping of ZGPD command ID to Zigbee ZCL command ID.
| zb_ret_t zb_zgp_convert_8bit_vector | ( | zb_uint8_t | vector_8bit_cmd_id, |
| zb_uint8_t | switch_type, | ||
| zb_uint8_t | num_of_contacts, | ||
| zb_uint8_t | contact_status, | ||
| zb_uint8_t * | zgp_cmd_out | ||
| ) |
The function may be overridden by the application to implement custom translation of 8-bit vector command (generic switch).
If this function is not implemented in the application, then ZBOSS performs a default translation as recommended by ZGP spec (see Green Power Basic specification v1.1.1, tables 51, 52). If no default translation is found, the received command will be dropped.
If this function is implemented in the application, then the application is fully responsible for a translation of GPD 8-bit vector commands. For any return code but RET_OK, ZBOSS will stop command processing and drop it.
| [in] | vector_8bit_cmd_id | - incoming command ID: press (0x69) or release (0x6a) |
| [in] | switch_type | - switch type of the command's originator (see ZGP spec. A.4.2.1.1.10) |
| [in] | num_of_contacts | - number of contacts, which command's originator provides |
| [in] | contact_status | - contact status from the payload of the received command |
| [out] | zgp_cmd_out | - GPDF command ID, to which incoming command should be translated |
| RET_OK | - on successful translation |
| RET_ERROR | - on failure |
| zb_uint8_t zb_zgp_get_skip_gpdf | ( | void | ) |
Checks if ZBOSS skips all incoming GPDFs.
| ZB_TRUE | - direct GPDF reception is ignored: device works always through the proxy |
| ZB_FALSE | - GPDF is processed: device works as a combo (default) |
| void zb_zgp_gpdf_raw_indication | ( | zb_bufid_t | buf_ref | ) |
Frees the incoming raw GPDF packet (buffer). This function can be overridden by the application to implement custom handling of the buffer.
If this function is implemented in the application, the application itself shall handle freeing the buffer; otherwise ZBOSS will drop the buffer without any additional handling.
| [in] | buf_ref | - buffer with incoming raw GPDF packet |
| void zb_zgp_set_shared_security_key | ( | zb_uint8_t * | key | ) |
Sets gpSharedSecurityKey GP cluster attribute.
Details are described in A.3.3.3.1 gpSharedSecurityKey attribute.
| [in] | key | - security key to set |
| void zb_zgp_set_shared_security_key_type | ( | zb_uint_t | key_type | ) |
Sets gpSharedSecurityKeyType GP cluster attribute.
Details are described in A.3.3.3.1 gpSharedSecurityKeyType attribute.
| [in] | key_type | - security key type to set (see zb_zgp_security_key_type_e()) |
| void zb_zgp_set_skip_gpdf | ( | zb_uint8_t | skip | ) |
Sets ZBOSS to skip all incoming GPDFs.
| [in] | skip |
|
ZB_TRUE parameter to prevent Combo device from receiving GPDFs, thus always working through the Proxy device. | void zb_zgp_sync_pib | ( | zb_uint8_t | param | ) |
Calls MLME-SET.request to sync SKIP_ALL_GPF attribute.
| [in] | param | - reference to the free buffer |
| void zb_zgps_accept_commissioning | ( | zb_bool_t | accept | ) |
Accepts/rejects ZGPD commissioning attempt.
This function should be called as an answer to commissioning request made by stack via ZB_ZGP_SIGNAL_APPROVE_COMMISSIONING signal or zb_zgp_comm_req_cb_t() callback.
Also, it can be called from zb_zgp_comm_req_cb_t() callback as well as outside it.
| [in] | accept |
|
| void zb_zgps_delete_all_zgpd | ( | void | ) |
Removes all information about all ZGPDs from the stack.
This function clears proxy, sink, mapping tables and TX queue.
| void zb_zgps_delete_zgpd | ( | zb_uint8_t | buf_ref, |
| zb_zgpd_id_t * | zgpd_id | ||
| ) |
Removes all information about ZGPD from the stack.
In ZGP, there is no way to instruct the ZGPD to leave the network. ZGPD can leave the network on its own using the "Decommissioning" command, but ZGPD may miss this command if it was not in the commissioning state.
This function removes all information related to the specified ZGPD from the stack.
| [in] | buf_ref | - reference to the free buffer |
| [in] | zgpd_id | - pointer to the identifier of the ZGPD to be removed |
zgpd_id after call. | void zb_zgps_get_diag_data | ( | zb_zgpd_id_t * | zgpd_id, |
| zb_uint8_t * | lqi, | ||
| zb_int8_t * | rssi | ||
| ) |
Retrieves LQI and RSSI last received from the ZGPD.
If there is no zgpd_id, ZB_MAC_LQI_UNDEFINED and ZB_MAC_RSSI_UNDEFINED will be set respectively.
| [in] | zgpd_id | - pointer to the ZGPD identifier |
| [out] | lqi | - pointer to store the ZGPD's LQI |
| [out] | rssi | - pointer to store the ZGPD's RSSI |
| zb_uint8_t zb_zgps_get_security_level | ( | void | ) |
Gets gpsSecurityLevel GP cluster attribute of the GPCB.
Details are described in A.3.3.2.6 gpsSecurityLevel attribute.
| void zb_zgps_set_commissioning_exit_mode | ( | zb_uint_t | cem | ) |
Sets gpsCommissioningExitMode GP cluster attribute.
Details are described in A.3.3.2.4 gpsCommissioningExitMode attribute.
| [in] | cem | - commissioning exit mode to set (see zgp_commissioning_exit_mode_t()) |
| void zb_zgps_set_communication_mode | ( | zgp_communication_mode_t | mode | ) |
Sets gpsCommunicationMode GP cluster attribute of the GPCB.
Details are described in A.3.3.2.3 gpsCommunicationMode attribute.
| [in] | mode | - communication mode to set (see zgp_communication_mode_t()) |
| void zb_zgps_set_security_level | ( | zb_uint_t | level | ) |
Sets gpsSecurityLevel GP cluster attribute of GPCB.
Details are described in A.3.3.2.6 gpsSecurityLevel attribute.
| [in] | level | - security level to set |
| void zb_zgps_start_commissioning | ( | zb_time_t | timeout | ) |
Puts ZGPS into the commissioning mode.
ZB_ZGP_SIGNAL_MODE_CHANGE is generated when sink changes mode from the operational mode to the commissioning mode and vice versa.
ZB_ZGP_SIGNAL_COMMISSIONING is generated if successful commissioning or decommissioning happens.
| [in] | timeout | - maximum commissioning time in beacon intervals
|
timeout parameter is different from 0 (timeout occurs).Action field set to 0x0 is received.| void zb_zgps_start_commissioning_on_ep | ( | zb_uint8_t | ep, |
| zb_time_t | timeout | ||
| ) |
Puts ZGPS into the commissioning mode on a specific endpoint.
| [in] | ep | - endpoint to start commissioning. Will be used for GPD command forwarding |
| [in] | timeout | - maximum commissioning time in beacon intervals
|
| void zb_zgps_stop_commissioning | ( | void | ) |
Switches ZGPS back to the operational mode from the commissioning mode.