Data Structures | |
| struct | zb_af_simple_desc_1_1_s |
| struct | zb_af_simple_desc_8_9_s |
Macros | |
| #define | ZB_AF_IS_EP_REGISTERED(_ep) ((zb_af_get_endpoint_desc( _ep ) != NULL)?(ZB_TRUE):(ZB_FALSE)) |
| Check endpoint registration in ZCL. More... | |
| #define | ZB_AF_START_DECLARE_ENDPOINT_LIST(ep_list_name) zb_af_endpoint_desc_t *ep_list_name[] = { |
| #define | ZB_AF_DECLARE_ENDPOINT_DESC( ep_name, ep_id, profile_id, reserved_length, reserved_ptr, cluster_number, cluster_list, simple_desc, rep_count, rep_ctx, lev_ctrl_count, lev_ctrl_ctx) |
| Initialize endpoint descriptor. More... | |
| #define | ZB_AF_FINISH_DECLARE_ENDPOINT_LIST } |
| #define | ZB_AF_SET_ENDPOINT_HANDLER(endpoint, handler) (zb_af_get_endpoint_desc((endpoint))->device_handler = (handler)) |
| Allows application to register cluster commands handler for a specific endpoint. More... | |
| #define | ZB_AF_SET_IDENTIFY_NOTIFICATION_HANDLER(endpoint, handler) (zb_af_get_endpoint_desc((endpoint))->identify_handler = (handler)) |
| Sets identify notification handler for endpoint. More... | |
| #define | ZB_ZCL_CLUSTER_DESC(cluster_id, attr_count, attr_desc_list, cluster_role_mask, manuf_code) |
| #define | ZB_AF_DECLARE_DEVICE_CTX(device_ctx_name, ep_list_name, ep_count, reporting_attr_count) |
| #define | ZB_AF_DECLARE_DEVICE_CTX_NO_REP(device_ctx_name, ep_list_name, ep_count) |
| #define | ZBOSS_DEVICE_DECLARE_REPORTING_CTX(rep_ctx, rep_count) zb_zcl_reporting_info_t rep_ctx[rep_count] |
| #define | ZBOSS_DEVICE_DECLARE_LEVEL_CONTROL_CTX(lev_ctrl_ctx, lev_ctrl_count) zb_zcl_cvc_alarm_variables_t lev_ctrl_ctx[lev_ctrl_count] |
| #define | ZBOSS_DECLARE_DEVICE_CTX(device_ctx_name, ep_list_name, ep_count) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_1_EP(device_ctx_name, ep_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_2_EP(device_ctx_name, ep1_name, ep2_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_3_EP(device_ctx_name, ep1_name, ep2_name, ep3_name) |
| #define | ZBOSS_DECLARE_DEVICE_CTX_4_EP(device_ctx_name, ep1_name, ep2_name, ep3_name, ep4_name) |
| #define | ZB_AF_REGISTER_DEVICE_CTX(_device_ctx) zb_af_register_device_ctx(_device_ctx) |
| #define | ZB_ZCL_REGISTER_DEVICE_CB(func_ptr) |
| Set Device user application callback. The macro sets a callback being called upon to need inform User App about change device attribute or need to execute H/W command. More... | |
Typedefs | |
| typedef struct zb_af_simple_desc_1_1_s | zb_af_simple_desc_1_1_t |
| typedef struct zb_af_simple_desc_8_9_s | zb_af_simple_desc_8_9_t |
| typedef zb_uint8_t(* | zb_device_handler_t) (zb_uint8_t param) |
| typedef void(* | zb_af_transmission_res_cb_t) (zb_uint8_t status) |
Functions | |
| zb_af_endpoint_desc_t * | zb_af_get_endpoint_desc (zb_uint8_t ep_id) |
| Search for endpoint (device) descriptor by endpoint ID. More... | |
| void | zb_apsde_data_indication_cont (zb_uint8_t param) |
| void | zb_af_set_data_indication (zb_device_handler_t cb) |
| Set up application callback to be called for APS data packets. More... | |
| void | zb_bdb_reset_via_local_action (zb_uint8_t param) |
| Perform "Reset with a Local Action" procedure (as described in BDB spec, chapter 9.5). The device will perform the NLME leave and clean all Zigbee persistent data except the outgoing NWK frame counter and application datasets (if any). The reset can be performed at any time once the device is started (see zboss_start). After the reset, the application will receive the ZB_ZDO_SIGNAL_LEAVE signal. More... | |
| void | zb_bdb_initiate_tc_rejoin (zb_uint8_t param) |
| Starts TC rejoin procedure. More... | |
| #define ZB_AF_DECLARE_DEVICE_CTX | ( | device_ctx_name, | |
| ep_list_name, | |||
| ep_count, | |||
| reporting_attr_count | |||
| ) |
WARNING: This API is deprecated, use ZBOSS_DECLARE_DEVICE_CTX instead.
| #define ZB_AF_DECLARE_DEVICE_CTX_NO_REP | ( | device_ctx_name, | |
| ep_list_name, | |||
| ep_count | |||
| ) |
WARNING: This API is deprecated, use ZBOSS_DECLARE_DEVICE_CTX instead.
| #define ZB_AF_DECLARE_ENDPOINT_DESC | ( | ep_name, | |
| ep_id, | |||
| profile_id, | |||
| reserved_length, | |||
| reserved_ptr, | |||
| cluster_number, | |||
| cluster_list, | |||
| simple_desc, | |||
| rep_count, | |||
| rep_ctx, | |||
| lev_ctrl_count, | |||
| lev_ctrl_ctx | |||
| ) |
Initialize endpoint descriptor.
| ep_name | - endpoint name |
| ep_id | - endpoint ID |
| profile_id | - ID of profile deployed on this endpoint |
| reserved_length | - unused parameter |
| reserved_ptr | - unused parameter |
| cluster_number | - number of clusters deployed on endpoint |
| cluster_list | - pointer to cluster list |
| simple_desc | - pointer to simple descriptor |
| rep_count | - maximum number of attributes that are being reported on a device |
| rep_ctx | - reporting context variable name (NULL if no reporting context) |
| lev_ctrl_count | - number of level control attributes |
| lev_ctrl_ctx | - level control context variable name (NULL if no level control context) |
| #define ZB_AF_FINISH_DECLARE_ENDPOINT_LIST } |
Finishes endpoint list declaration
| #define ZB_AF_IS_EP_REGISTERED | ( | _ep | ) | ((zb_af_get_endpoint_desc( _ep ) != NULL)?(ZB_TRUE):(ZB_FALSE)) |
Check endpoint registration in ZCL.
| _ep | - identifier of the endpoint under consideration. |
| #define ZB_AF_REGISTER_DEVICE_CTX | ( | _device_ctx | ) | zb_af_register_device_ctx(_device_ctx) |
Register device context.
| _device_ctx | - Pointer to the device context |
Example:
| #define ZB_AF_SET_ENDPOINT_HANDLER | ( | endpoint, | |
| handler | |||
| ) | (zb_af_get_endpoint_desc((endpoint))->device_handler = (handler)) |
Allows application to register cluster commands handler for a specific endpoint.
| endpoint | - Endpoint number |
| handler | - Pointer to a function, function type zb_device_handler_t |
| #define ZB_AF_SET_IDENTIFY_NOTIFICATION_HANDLER | ( | endpoint, | |
| handler | |||
| ) | (zb_af_get_endpoint_desc((endpoint))->identify_handler = (handler)) |
Sets identify notification handler for endpoint.
Utilized by ZCL Identify cluster
| endpoint | number |
| handler | to set |
| #define ZB_AF_START_DECLARE_ENDPOINT_LIST | ( | ep_list_name | ) | zb_af_endpoint_desc_t *ep_list_name[] = { |
General macro to declare endpoint description list
| ep_list_name | - name of ep list structure |
| #define ZB_ZCL_CLUSTER_DESC | ( | cluster_id, | |
| attr_count, | |||
| attr_desc_list, | |||
| cluster_role_mask, | |||
| manuf_code | |||
| ) |
| #define ZB_ZCL_REGISTER_DEVICE_CB | ( | func_ptr | ) |
Set Device user application callback. The macro sets a callback being called upon to need inform User App about change device attribute or need to execute H/W command.
| func_ptr | - a callback to set (of type zb_callback_t). |
Example:
| #define ZBOSS_DECLARE_DEVICE_CTX | ( | device_ctx_name, | |
| ep_list_name, | |||
| ep_count | |||
| ) |
Declare application's device context
| device_ctx_name | - device context variable name |
| ep_list_name | - name of endpoint list |
| ep_count | - number of supported endpoints |
| #define ZBOSS_DECLARE_DEVICE_CTX_1_EP | ( | device_ctx_name, | |
| ep_name | |||
| ) |
Declare application's device context for single-endpoint device
| device_ctx_name | - device context variable name |
| ep_name | - variable holding endpoint context |
| #define ZBOSS_DECLARE_DEVICE_CTX_2_EP | ( | device_ctx_name, | |
| ep1_name, | |||
| ep2_name | |||
| ) |
Declare application's device context for two-endpoint device
| device_ctx_name | - device context variable name |
| ep1_name | - variable holding context for endpoint 1 |
| ep2_name | - variable holding context for endpoint 2 |
| #define ZBOSS_DECLARE_DEVICE_CTX_3_EP | ( | device_ctx_name, | |
| ep1_name, | |||
| ep2_name, | |||
| ep3_name | |||
| ) |
Declare application's device context for three-endpoint device
| device_ctx_name | - device context variable name |
| ep1_name | - variable holding context for endpoint 1 |
| ep2_name | - variable holding context for endpoint 2 |
| ep3_name | - variable holding context for endpoint 3 |
| #define ZBOSS_DECLARE_DEVICE_CTX_4_EP | ( | device_ctx_name, | |
| ep1_name, | |||
| ep2_name, | |||
| ep3_name, | |||
| ep4_name | |||
| ) |
Declare application's device context for for-endpoint device
| device_ctx_name | - device context variable name |
| ep1_name | - variable holding context for endpoint 1 |
| ep2_name | - variable holding context for endpoint 2 |
| ep3_name | - variable holding context for endpoint 3 |
| ep4_name | - variable holding context for endpoint 4 |
| #define ZBOSS_DEVICE_DECLARE_LEVEL_CONTROL_CTX | ( | lev_ctrl_ctx, | |
| lev_ctrl_count | |||
| ) | zb_zcl_cvc_alarm_variables_t lev_ctrl_ctx[lev_ctrl_count] |
Declare device level control context
| lev_ctrl_ctx | - level control context variable name |
| lev_ctrl_count | - number of level control attributes |
| #define ZBOSS_DEVICE_DECLARE_REPORTING_CTX | ( | rep_ctx, | |
| rep_count | |||
| ) | zb_zcl_reporting_info_t rep_ctx[rep_count] |
Declare device reporting context
| rep_ctx | - reporting context variable name |
| rep_count | - number of reporting attributes |
| typedef struct zb_af_simple_desc_1_1_s zb_af_simple_desc_1_1_t |
General descriptor type
| typedef struct zb_af_simple_desc_8_9_s zb_af_simple_desc_8_9_t |
| typedef void(* zb_af_transmission_res_cb_t) (zb_uint8_t status) |
Callback for notifying user about status of ZCL/ZDO command transmission
| typedef zb_uint8_t(* zb_device_handler_t) (zb_uint8_t param) |
Device command handler
| param | - index of buffer with ZCL command |
| zb_af_endpoint_desc_t* zb_af_get_endpoint_desc | ( | zb_uint8_t | ep_id | ) |
Search for endpoint (device) descriptor by endpoint ID.
| ep_id | - identifier of the endpoint. |
| void zb_af_set_data_indication | ( | zb_device_handler_t | cb | ) |
Set up application callback to be called for APS data packets.
That API call may be useful for tests which uses custom profile id or which needs to send raw data over APS.
| cb | - callback to call when AF got APS packet. zb_apsde_data_indication_t |
Example:
| void zb_apsde_data_indication_cont | ( | zb_uint8_t | param | ) |
Continue inconimg packet proicessing after ZG->zdo.af_data_cb returned TRUE
| param | - incoming packet. Be sure it was initially passed to ZG->zdo.af_data_cb. |
| void zb_bdb_initiate_tc_rejoin | ( | zb_uint8_t | param | ) |
Starts TC rejoin procedure.
If device doesn't have a TCLK and UnsecureTcRejoinEnabled policy is set to ZB_FALSE (this is the default setting), TC rejoin won't be performed and ZB_BDB_SIGNAL_TC_REJOIN_DONE signal with RET_ERROR status will be raised.
| param | - buffer reference (if 0, buffer will be allocated automatically) |
| void zb_bdb_reset_via_local_action | ( | zb_uint8_t | param | ) |
Perform "Reset with a Local Action" procedure (as described in BDB spec, chapter 9.5). The device will perform the NLME leave and clean all Zigbee persistent data except the outgoing NWK frame counter and application datasets (if any). The reset can be performed at any time once the device is started (see zboss_start). After the reset, the application will receive the ZB_ZDO_SIGNAL_LEAVE signal.
| param | - buffer reference (if 0, buffer will be allocated automatically) |