Logo
Developing with ZBOSS for Zigbee
Tunneling cluster attributes

Data Structures

struct  zb_zcl_tunneling_attrs_s
 Tunneling cluster attributes. More...
 

Macros

#define ZB_ZCL_TUNNELING_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)
 Default value for Tunneling cluster revision global attribute. More...
 
#define ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_MIN_VALUE   0x0001
 Min value for the CloseTunnelTimeout attribute. More...
 
#define ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_DEFAULT_VALUE   0xFFFF
 Default value for the CloseTunnelTimeout attribute. More...
 
#define ZB_ZCL_DECLARE_TUNNELING_ATTRIB_LIST(attr_list, close_tunnel_timeout)
 Declare attribute list for Tunneling cluster. More...
 
#define ZB_ZCL_DECLARE_TUNNELING_ATTR_LIST(attr_list, attrs)   ZB_ZCL_DECLARE_TUNNELING_ATTRIB_LIST(attr_list, &attrs.close_tunnel_timeout )
 Declare attribute list for Tunneling cluster cluster. More...
 

Typedefs

typedef struct zb_zcl_tunneling_attrs_s zb_zcl_tunneling_attrs_t
 Tunneling cluster attributes. More...
 

Enumerations

enum  zb_zcl_tunneling_attr_e { ZB_ZCL_ATTR_TUNNELING_CLOSE_TUNNEL_TIMEOUT_ID = 0 }
 Tunneling cluster attribute identifiers. More...
 

Detailed Description

Macro Definition Documentation

§ ZB_ZCL_DECLARE_TUNNELING_ATTR_LIST

#define ZB_ZCL_DECLARE_TUNNELING_ATTR_LIST (   attr_list,
  attrs 
)    ZB_ZCL_DECLARE_TUNNELING_ATTRIB_LIST(attr_list, &attrs.close_tunnel_timeout )

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_tunneling.h>

Declare attribute list for Tunneling cluster cluster.

Parameters
[in]attr_list- attribute list variable name
[in]attrs- pointer to zb_zcl_tunneling_attrs_s structure

§ ZB_ZCL_DECLARE_TUNNELING_ATTRIB_LIST

#define ZB_ZCL_DECLARE_TUNNELING_ATTRIB_LIST (   attr_list,
  close_tunnel_timeout 
)

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_tunneling.h>

Value:
ZB_ZCL_START_DECLARE_ATTRIB_LIST_CLUSTER_REVISION(attr_list, ZB_ZCL_TUNNELING) \
ZB_ZCL_SET_ATTR_DESC(ZB_ZCL_ATTR_TUNNELING_CLOSE_TUNNEL_TIMEOUT_ID, (close_tunnel_timeout)) \
ZB_ZCL_FINISH_DECLARE_ATTRIB_LIST
CloseTunnelTimeout defines the minimum number of seconds that the server waits on an inactive tunnel ...
Definition: zb_zcl_tunneling.h:66

Declare attribute list for Tunneling cluster.

Parameters
[in]attr_list- attribute list name
[in]close_tunnel_timeout- pointer to variable to store On/Tunneling attribute value

§ ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_DEFAULT_VALUE

#define ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_DEFAULT_VALUE   0xFFFF

§ ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_MIN_VALUE

#define ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_MIN_VALUE   0x0001

§ ZB_ZCL_TUNNELING_CLUSTER_REVISION_DEFAULT

#define ZB_ZCL_TUNNELING_CLUSTER_REVISION_DEFAULT   ((zb_uint16_t)0x0002u)

Typedef Documentation

§ zb_zcl_tunneling_attrs_t

Enumeration Type Documentation

§ zb_zcl_tunneling_attr_e

#include </conan-data/ti_zigbee/9.14.00.04/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_tunneling.h>

Tunneling cluster attribute identifiers.

See also
SE spec, subclause D.6.2.2
Enumerator
ZB_ZCL_ATTR_TUNNELING_CLOSE_TUNNEL_TIMEOUT_ID 

CloseTunnelTimeout defines the minimum number of seconds that the server waits on an inactive tunnel before closing it on its own and freeing its resources (without waiting for the CloseTunnel command from the client). Inactive means here that the timer is re-started with each new reception of a command.0x0000 is an invalid value.

See also
ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_MIN_VALUE
ZB_ZCL_TUNNELING_CLOSE_TUNNEL_TIMEOUT_DEFAULT_VALUE